Using S32K148EVB as Flasher/Debugger for external S32K148 based custom hardware using OpenSDA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using S32K148EVB as Flasher/Debugger for external S32K148 based custom hardware using OpenSDA

跳至解决方案
1,163 次查看
vijayvaidya
Contributor I

Hello,

After going through the schematic for the said EVB (S32K148EVB-SCH-29644-RB.pdf), we find that the EVB 'can be' used to Flash/Debug a S32K148 based external custom hardware, through J20 connector and managing 'Isolation Resistors'

But there is no specific mention of this facility either in Quick Start Guide (S32K148EVB-QSG.pdf) or User Manual (S32K148-UM.pdf).

Can somebody confirm this and if yes, with what modifications.

We intend to use the EVB that is available with us for this intended application for our new project based on S32K148.

Thank you very much

Regards,

- Vijay Vaidya

 

 

0 项奖励
回复
1 解答
1,137 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

I'm afraid it can not achieve.

You can refer this: Can't flash elf to S32K146Q100 by OpenSDA

 

Best Regards,
Robin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,138 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

I'm afraid it can not achieve.

You can refer this: Can't flash elf to S32K146Q100 by OpenSDA

 

Best Regards,
Robin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,127 次查看
vijayvaidya
Contributor I

Hello,

Thanks Robin_Shen for your inputs.

Regards,

- Vijay Vaidya

 

 

0 项奖励
回复