Why is the Rx FIFO Transfer Type option invalid in my S32DS3.5 (RTD3.0.0) project, but it is valid and optional in the S32DS3.4 (RTD2.0.0) project downloaded from the NXP community
解決済! 解決策の投稿を見る。
Hi,
I see transfer type can be selected, but here an error is different.
When Legacy FIFO is enabled then CAN FD cannot be used.
BR, Petr
Hi,
if you have CAN FD enabled then only Enhanced RXFIFO can be used. This is only available on FlexCAN0, so that's why option for transfer type is greyed.
If you disable CAN FD and enable Legacy RxFIFO then you will have this option accessible.
BR, Petr
But,my Flexcan_0 can not do it too.
Hi,
I see transfer type can be selected, but here an error is different.
When Legacy FIFO is enabled then CAN FD cannot be used.
BR, Petr