Dear Sir,
Recently, when I was using RTD 4.0, I found that the FLS module was not available for selection in a new project. The version I installed is: SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip. Screenshot below:
Is it possible that the FLS module in the new version of RTD has been replaced by INFLS and EXFLS modules?
Thanks!
Hi
Because this RTD is based on AUTOSAR R21-11, there is no FLS module.
Please refer to the discussion in no fee and fls modules in RTD of s32k3x
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------