Hi, noob here.
About TJA1145T/FD,I have a question:
I have refer to several designs with TJA1145T and I found that the 1145 communicates with microcontroller through SPI.If I follow the hardware design of 1145 but not send any SPI frame to 1145 when I power on the MCU board(In SW not initial the 1145),is the 1145 in operating mode or can MCU transmit and receive CAN frames by 1145?
I have code of a S32K application which uses UJA1169. However,there is no code about UJA1169 initial and SPI communication with microcontroller ,but it can still transfer CAN data.
You reply will be highly appreciated.Thanks.
解決済! 解決策の投稿を見る。
Hi,
upon power on TJA1145 enters Standby mode with CAN transceiver disabled, you need to send command over SPI. That is put TJA1145 in Normal mode (MC = 111) and enable CAN transceiver by setting bits CMC in the CAN control register to 01 or 10.
BR, Petr
Hi,
upon power on TJA1145 enters Standby mode with CAN transceiver disabled, you need to send command over SPI. That is put TJA1145 in Normal mode (MC = 111) and enable CAN transceiver by setting bits CMC in the CAN control register to 01 or 10.
BR, Petr