StandardTypes.h: No such file or directory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

StandardTypes.h: No such file or directory

Jump to solution
532 Views
Silvano
Contributor I

Hello,

I have this error when I try to build the project : 

Silvano_0-1709639789376.png

 

I installed RTD version 4.0.0 to use the package for S32K396-LQFP

Silvano_1-1709639874763.png

I also tried to insert manually all the <file_name>.h in the includes folder from the workspace but I still have errors.

Could you help me please ?:

 

Silvano_2-1709640662945.pngSilvano_3-1709640677066.png

Silvano_0-1709641697298.png

 

 

0 Kudos
Reply
1 Solution
506 Views
spara7c5
Contributor III

For sure you don t need to install Tresos.
It s seems there is some conflicts in your S32DS package manager. Try to remove all extensions, then install only RTD 4.0.0 and run "Project from example"

View solution in original post

0 Kudos
Reply
4 Replies
508 Views
Silvano
Contributor I

Hello @spara7c5 

Yes , I am trying to compile the example project. 

I have this issue since I installed the "RTD AUTOSAR R21-11 Version 4.0.0 HF01 " and it was working normally with the version 3.0.0.

Do you think I should install EB tresos Studio 29.0.0 ?

0 Kudos
Reply
507 Views
spara7c5
Contributor III

For sure you don t need to install Tresos.
It s seems there is some conflicts in your S32DS package manager. Try to remove all extensions, then install only RTD 4.0.0 and run "Project from example"

0 Kudos
Reply
501 Views
Silvano
Contributor I
It was the problem, thank you!
There was a conflict between version 3.0 and 4.0
0 Kudos
Reply
523 Views
spara7c5
Contributor III

Hello Silvano,
I faced the same issue like you and it was for an unmatch between tresos RTD version and S32DS installed RTD. Are you trying to compile the example project? they work out of the box

0 Kudos
Reply