S32k358 SBC_fs26 module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32k358 SBC_fs26 module

5,120 次查看
mariam
Contributor I

S32k358 I work on SBC_fs26 and I found this error ('Sbc_fs26_PBCfgVariantPredefined' undeclared (first use in this function)), taking in consideration that we are working using precompile option 

0 项奖励
回复
26 回复数

4,412 次查看
mariam
Contributor I

I noticed that the value for " -Dcom.nxp.swtools.codegenscript.timeout=60000 " is different . It's currently set to a different value.
Do I need to change this value??

0 项奖励
回复

4,402 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Mariam,

I am not sure, why the " -Dcom.nxp.swtools.codegenscript.timeout=60000 " line appeared in your S32DS.ini file. I have checked my S32DS.ini file and I don't have the line there. Please rewrite the " -Dcom.nxp.swtools.codegenscript.timeout=60000 " with the recommended -"Dcom.nxp.swtools.codegenscript.timeout=-1"

JozefKozon_0-1697004297291.png

With Best Regards,

Jozef

0 项奖励
回复

4,289 次查看
mariam
Contributor I

I followed the provided steps, but the issue still exist.
Considering that we have attempted S32DS without any noticeable changes.

0 项奖励
回复

4,438 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Mariam,

please see a solution below, where another customer had similar issue. 

DESCRIPTION

There can be multiple reasons for the failure, here is a list:

  1. Installation order form the HVBMS installation guide was not followed, BMS SDK was installed first then RTD.
  2. Generation timeout of S32DS in order to fix this issue see section : 5.1.1.8.3.1 form the HVBMS installation guide.

“In case of difficulties in the code generation using S32 Configuration due to computer speed, it is possible to remove the timeout in the C:\NXP\S32DS.3.4\eclipse\s32ds.ini file by adding the following line: -Dcom.nxp.swtools.codegenscript.timeout=-1.”

Or if you are using the S32DS version 3.5, then in C:\NXP\S32DS.3.5\eclipse\s32ds.ini

After adding this in .ini file please restart S32DS and create a new workspace where a fresh import has to be tried.

With Best Regards,

Jozef

 

0 项奖励
回复

4,262 次查看
MarinaMagdy
Contributor I

Hi Jozef,
Thanks for your support but I have concerns:
1-We are configuring from Tresos tool, not design studio.
2-Also it is noticed that SBC_FS26_CONFIG_EXT define has no replacement parameter in the generated file CDD_Sbc_Fs26_Cfg.h

It is only generated correctly through Design studio

 

Below screenshot from configuration through Tresos

MarinaMagdy_0-1699870466044.png

 

Following screenshot from configuring through design studio

MarinaMagdy_0-1699877489887.png

 


Note:
SBC package version: S32K3_FS26_R21-11_2.0.0_CD01

 

0 项奖励
回复

4,237 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Marina,

I have contacted an application team for an advice. So far there is no answer from them. As soon as they answer me, I will definitely reply to you.

Thank you for your patience.

With Best Regards,

Jozef

0 项奖励
回复

4,195 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Marina,

I apologize for a late reply. The application team have informed me, that they are working on the case. As soon as they send me another answer, I will definitely reply to you.

Thank you for your patience.

With Best Regards,

Jozef

0 项奖励
回复

4,184 次查看
MarinaMagdy
Contributor I
Hi Jozef,
We appreciate your response, and looking forward to hearing from you regarding our question.
0 项奖励
回复

4,177 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Marina,

please see a suggestion from the application team. Please test it.

DESCRIPTION

I think the problem is that the customer did not clicked on the Post Build Variant Used check box.

JozefKozon_0-1700654659414.png

 Can they try this and see if the error is still there?

With Best Regards,

Jozef

0 项奖励
回复

4,172 次查看
MarinaMagdy
Contributor I
Hi Jozef,
Tested and the same issue still exist.
0 项奖励
回复

4,146 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Marina,

please see below an answer from the application team.

DESCRIPTION

Please tell the customer to update to the RTM version of the SBC_FS26, SW32K3_FS26_R21-11_2.0.0_D2308, it is compatible with RTD 3.0.0.  And configure the SBC as it follows.

JozefKozon_0-1700804705708.png

This is avaiable in the bundle in package manager S32K358 HVBMS: Automotive Software Package Manager | NXP Semiconductors 

 

JozefKozon_1-1700804705848.png

With Best Regards,

Jozef

 

 

0 项奖励
回复

4,097 次查看
mariam
Contributor I

I can't install it ! 

0 项奖励
回复

4,082 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Mariam,

are you able to generate the Bundle Installer? Please share a printscreen view, of the Package Manager. How you see it on your side.

JozefKozon_0-1701235569389.png

With Best Regards,

Jozef

 

0 项奖励
回复

4,069 次查看
mariam
Contributor I

this package for s32k344 not s32k358 

0 项奖励
回复

4,056 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Mariam,

thank you for the update. Could you please confirm the software and hardware you are using? 

Please state the full Evaluation Board number you are using. Is it RD-K358BMU or RD-K344BMU, or any other? Or are you working on your own board?

Which S32DS IDE you are using? 3.4 or 3.5? 

JozefKozon_0-1701327439504.pngJozefKozon_1-1701327459959.png

With Best Regards,

Jozef

 

 

 

0 项奖励
回复

4,049 次查看
mariam
Contributor I

using S32k3X8EVB-Q289 "SCH-89070 REV A3" 
Design studio version 3.5

0 项奖励
回复

4,030 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Mariam,

thank you very much for confirmation. This clears out, why you cannot download the recommended software. It seems you do not have a license for it. The license comes with HVBMS EVBs. So you are not using our RD-K358BMU EVB for HVBMS. This is question for different application team. I have contacted the other team. As soon as they answer me, I will definitely reply to you. 

Thank you for your patience. 

With Best Regards,

Jozef

0 项奖励
回复

4,022 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Mariam,

the application team suggests to use S32K3 FS26 RTM version. I have download it for you. Please find it attached. 

JozefKozon_0-1701431759686.png

DESCRIPTION

I see the issue was reported on version 2.0.0 CD01

Can you please suggest they try 2.0.0 RTM instead?

With Best Regards,

Jozef

0 项奖励
回复

3,939 次查看
mariam
Contributor I

the issue still exist 

0 项奖励
回复

3,932 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Mariam,

do you receive the same error ('Sbc_fs26_PBCfgVariantPredefined' undeclared (first use in this function)) with the S32K3 FS26 RTM version software? Or is there an other error message?

With Best Regards,

Jozef

0 项奖励
回复