Hello,
I am using s32k148 chip. When reading the SAI Rx FIFOs, I am getting pointer values greater than 7.
The S32K Reference Manual specifies, that each receive channel has a FIFO of 8 units (each unit 32-bit size). The manual also specifies, that in SAI RFRn register WFP and RFP have 4-bit size, which is more than required to store 0-7 write/read pointer.
Are the FIFOs bigger than 8 units? Is it normal to observe Rx WFP values larger than 7?
Thank you,
Jakub
Hai jakub,
could you please tell me which microphone have you used for SM32K148 ??
if possible could you share the details, how to configuration microphone ??
Thanks
saichand
Hi Jakub,
Sorry for the delay.
We have been trying to reproduce that without any success.
The FIFO pointers show values in the range 0-8 as expected.
Could you share a screenshot of the registers with the FIFO pointers?
Also, what SAI configuration do you use?
The more information, the better.
The SAI initialization code or a test project would be great.
Thanks,
Daniel
Hello Jakub,
Thanks for the additional information and sorry for the delay.
Unfortunately, the issue is still under discussion with design.
Also, we have still difficulties to reproduce the bahaviour for some reason.
If possible, could you share a working test code, the whole project?
You could send it via a ticket if you don't want to post it here.
Anyway, I will update this thread once we have confirmation from the IP designer.
Thanks,
Daniel
Hello Daniel,
I don't have a sample project which I could share. I only have my full application.
Would register dump from S32 Design Studio help? If yes, then I can post one, just let me know which registers you need.
Thanks,
Jakub
Hello Jakub,
UPDATE,
I'm sorry for the delayed response and confusing information.
The FIFO pointers are circular. Although the FIFO size is 8 words, the pointers increment up to 0xF.
The number of words in the FIFO is then the relative difference between the WFP, RFP pointers.
Let say 5 words is written to the Receive FIFO by the HW, then, the RFRn_WFP pointer shows 0x5 while the RFRn_RFP pointer shows 0x0 until all the data are read (by DMA, for example) from the FIFO, then the RFRn_RFP is also 0x5.
And because at this point the pointers are identical, the FIFO is empty.
If other 5 words are received, the RFRn_WFP pointer increments to 0xA while the RFRn_RFP pointer stays at 0x5 until the data (5 words) are read from the FIFO, then the RFRn_RFP also increments to 0xA.
And because at this point the pointers are identical, the FIFO is empty again and a new transfer can be initialized.
This is a correction of my previous answer - the FIFO does not need to be reset. I’m sorry for that.
You can refer to the sai_transfer_s32k148 SDK example, this example utilizes DMA.
The FIFOs are reset during initialization in the SAI_DRV_RxInit(), SAI_DRV_TxInit() funtions only.
Regards,
Daniel