S32k144EVB - Q100 is not detected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32k144EVB - Q100 is not detected

1,103 Views
AparnaSridharan
Contributor II

Hi,

I am having S32k144EVB-Q100 board. I connected the evb board with my laptop it is detected.

AparnaSridharan_0-1648887501545.png

But when I tried to flash the code, it shows error connecting with my board. What might me be the problem.

AparnaSridharan_1-1648887590299.png

This is the debug configuration i have used.

AparnaSridharan_2-1648887978839.png

 

0 Kudos
Reply
3 Replies

1,075 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

is that brand new board?

What is the connection of J107 jumper? Do you use external power supply or USB cable only? If the position of the jumper is 1-2, the board is powered by USB cable only, if it is 2-3, external 12V needs to be connected.

Regards,

Lukas

0 Kudos
Reply

1,071 Views
AparnaSridharan
Contributor II

hi @lukaszadrapa ,

I have connected jumper J107 in position 1-2. Through USB cable i am connecting the board. I am not able to perform debug through Open SDA. But when I connect jumper in 2-3 position and powered through 12V I can debug using PE micro programmer. I am not able to perform debug when I connect through open SDA. 

0 Kudos
Reply

1,060 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 Kudos
Reply