Hi,
I am having S32k144EVB-Q100 board. I connected the evb board with my laptop it is detected.
But when I tried to flash the code, it shows error connecting with my board. What might me be the problem.
This is the debug configuration i have used.
Hi,
is that brand new board?
What is the connection of J107 jumper? Do you use external power supply or USB cable only? If the position of the jumper is 1-2, the board is powered by USB cable only, if it is 2-3, external 12V needs to be connected.
Regards,
Lukas
hi @lukaszadrapa ,
I have connected jumper J107 in position 1-2. Through USB cable i am connecting the board. I am not able to perform debug through Open SDA. But when I connect jumper in 2-3 position and powered through 12V I can debug using PE micro programmer. I am not able to perform debug when I connect through open SDA.
Could you try to follow this article?
Regards,
Lukas