S32k118 ADC Accuracy

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,542件の閲覧回数
종찬박
Contributor II

Hi 

I compared actual voltage to ADC value.

but, those value were quite different.

I proceeded as follows.

종찬박_0-1611623117761.png

could you tell me why calculating value is different with ADC value?

and do I have to what to check?

 

Regards,

Jongchan.

 

0 件の賞賛
返信
1 解決策
1,539件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Jongchan,

Please refer: AN12217, S32K1xx ADC guidelines, spec and configuration
The impedance of the analog signal source or series resistance (RIN) between the source and the input pin causes a voltage drop across it because of the current flowing into the pin. It can be understood as the resistance observed “looking out” of the ADC into the source driving the input signal to be sampled.

causes a voltage drop.png

For this reason, precautions must be taken to ensure that the analog input signal source resistance is within ADC specification. In the datasheet for S32K devices, this parameter can be found as Source Impedance (RS).Rs Source impedendance.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
897件の閲覧回数
Muskz
Contributor II

Can I understand it this way? If I use an adc clock that is less than 4M, the maximum allowable rs for external circuits is 5k.
If I use an adc clock of 40M, what should be the rs? Why is it not stated in the manual, should it be larger or smaller than 5k?

Thank you.

タグ(2)
0 件の賞賛
返信
1,540件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Jongchan,

Please refer: AN12217, S32K1xx ADC guidelines, spec and configuration
The impedance of the analog signal source or series resistance (RIN) between the source and the input pin causes a voltage drop across it because of the current flowing into the pin. It can be understood as the resistance observed “looking out” of the ADC into the source driving the input signal to be sampled.

causes a voltage drop.png

For this reason, precautions must be taken to ensure that the analog input signal source resistance is within ADC specification. In the datasheet for S32K devices, this parameter can be found as Source Impedance (RS).Rs Source impedendance.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信