S32K3 flash (c40asf): is it possible to cross a 128 bytes boundary?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 flash (c40asf): is it possible to cross a 128 bytes boundary?

Jump to solution
755 Views
ferencvalenta
Contributor III

Description from the manual:

"A flash memory program sequence operates on any page within the flash core. Within a page, up to eight words may be altered in a single program operation. Also, up to four pages can be altered in a single program operation. Whenever the array is programmed, the ECC bits also get programmed."

Is there any constraint for the 4 pages to be programmed with one operation? I played a bit with the flash controller, and it seems that the DATA registers are always mapped to 128-byte pages in the memory. That is, it's not possible to program addresses that cross a 128-bytes boundary, because an address 128 bytes lower would be programmed. The lower 7 bits of PEADR_P do not seem to have any effect on what address is programmed, basically the offset of the DATA register is ORed to PEADR_P to yield the effective programming address.

Is that normal or am I doing something wrong? I did not find a description how do the DATA registers map to memory locations relative to PEADR_P. This is a sort of limitations, because 4-page program operations must be aligned to 128 bytes?

Tags (3)
0 Kudos
Reply
1 Solution
733 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @ferencvalenta,

Up to four pages (maximum 128-byte of the program data buffer) can be programmed at once on a quad-page boundary (aligned to 128 bytes as well).

This means the data to be written must fall within a quad-page, we have to split the write operation based on that boundary.

In RTD 3.0.0 (C40_Ip driver) and newer versions, there is this condition:

Address Offset + Length <= C40_DATA_SIZE_BYTES_U32 (128 Bytes).

If not met, the driver reports an error.

This condition is not present in older RTD versions, and this may cause issues.

 

Regards,

Daniel

View solution in original post

1 Reply
734 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @ferencvalenta,

Up to four pages (maximum 128-byte of the program data buffer) can be programmed at once on a quad-page boundary (aligned to 128 bytes as well).

This means the data to be written must fall within a quad-page, we have to split the write operation based on that boundary.

In RTD 3.0.0 (C40_Ip driver) and newer versions, there is this condition:

Address Offset + Length <= C40_DATA_SIZE_BYTES_U32 (128 Bytes).

If not met, the driver reports an error.

This condition is not present in older RTD versions, and this may cause issues.

 

Regards,

Daniel