S32K3 core power down error & running(bus error)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K3 core power down error & running(bus error)

1,553 次查看
kjy106906
Contributor IV

I ask what state the MCU is in and what cases occur in the following situations.

What's interesting is that if I run a specific function with Over(Trace32), the issue occurs, but when I run it with Step(Trace32), the issue does not occur.

(Power is being supplied to the MCU normally.)

kjy106906_0-1713939415180.png

 

标记 (1)
0 项奖励
回复
11 回复数

1,542 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @kjy106906,

Can you be more specific?

What function do you step over here?

Can you also specify the MCU and RTD version if you use it?

 

Thank you,

BR, Daniel

0 项奖励
回复

1,535 次查看
kjy106906
Contributor IV

Thank you always @danielmartynek 

That function is not an RTD function but a simple calculation function.
An issue occurs when calculating the CRC of C40 read data at a specific address.
This occurs when executing the CRC calculation function, not when reading.
MCU: S32K312, RTD version: 2.0.0

 

I wonder what state the MCU is in and the reason for entering that state.

 

0 项奖励
回复

1,529 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @kjy106906,

Please find more information about the fault exception.

Refer to these documents:

https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447

https://community.nxp.com/t5/S32K-Knowledge-Base/How-To-Debug-A-Fault-Exception-On-ARM-Cortex-M-V7M-...

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-HARDFAULT-Handling-Interrupt-DS3-5-...

Read Configurable Fault Status Register (CSFR) and Bus Fault Address Register (BFAR) if BFARVALID = 1. You should be able to find the PC address of the fault instruction on the stack.

 

Regards,

Daniel

 

 

 

 

0 项奖励
回复

1,499 次查看
kjy106906
Contributor IV

Thank you

Even if I set a break on the error handler, the break does not occur and the MCU enters the corresponding state.

 

I wonder what state the MCU is in and the reason for entering that state.

0 项奖励
回复

1,490 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @kjy106906,

So, I understand the core does not detect any fault exception, it does not go to the HardFault_Handler().

Can you monitor the reset_b pin? Is the application running?

If so, it might be a lauterbach issue.

 

BR, Daniel

 

0 项奖励
回复

1,386 次查看
kjy106906
Contributor IV

Thank you @danielmartynek 

I am currently using Vector Microsar
The MCU does not enter any Os Hal Fault (Exception).
If an MCU Exception is entered, I think I will see the MCU jumping to the corresponding code in the debugger, but currently a Bus error is output in Trace32.
Therefore, it seems that an exception did not occur.
If there are any more points to check, let me know.


Neither Reset_b nor VDD_HA_A fall to Low.

This issue causes infinite SBC reset in BMS-only state without Trace32. Because that issue occurs in Dataflash Init, the MCU does not operate and an infinite reset of the SBC occurs.
So it's not a lauterbach issue either.

It's an important issue for us. Please let me know if there are any more points to check.

0 项奖励
回复

1,375 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @kjy106906,

I would like to test it on my side.

Can you share the project?

Or preferably a simplified version with .elf that can reproduce the issue?

If you don't want to share it here, create a ticket.

 

Thank you,

Daniel

 

0 项奖励
回复

1,365 次查看
kjy106906
Contributor IV

Thank you @danielmartynek 

Sharing the entire project is not possible due to company security reasons.
Even if I share my elf, it currently works on my board.
Testing may not be possible in your environment.

It is also not possible to share the simplified elf.
Strangely, even if I add a few lines of unnecessary code (adding a while statement for debugging, adding a global variable, etc.), the issue does not reproduce.

Currently, this issue has occurred in 5 BMS boards.
It's all related to Dataflash.
Could the above phenomenon occur due to dataflash area being broken or other errors?

0 项奖励
回复

1,338 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

When you read the DFlash, do you use the driver?

Because the driver checks for errors:

danielmartynek_0-1714660282009.png

 

Thank you,

Daniel

0 项奖励
回复

1,330 次查看
kjy106906
Contributor IV

Thank you @danielmartynek 

 

I'm also using the C40 library. (C40_Ip_Read)
However, Error is not returned, ( Success is returned.)

0 项奖励
回复

1,279 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @kjy106906,

You wrote: "Strangely, even if I add a few lines of unnecessary code (adding a while statement for debugging, adding a global variable, etc.), the issue does not reproduce."

If you write registers or an sram memory, can you read it back so that all the operations are properly serialized?

RM, rev.8, Section 3.8 Serialization of memory operations.

 

Regards,

Daniel

0 项奖励
回复