S32K3 ADC Filter Capacitance Selection Range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 ADC Filter Capacitance Selection Range

494件の閲覧回数
hongpingxu-b364
NXP Employee
NXP Employee

Hi,

 

On S32K3 Data Sheet, Figure 33 [SAR ADC Input Circuit].

SAR ADC Input Circuit.jpg

Could you please clarify the Filter Capacitance (CF) selection range. Is there any formula for this value?

Ps: S32K312 MCU Clock: 120 MHz, ADC clock speed: 80 MHz

 

BR,

Hornby

0 件の賞賛
返信
1 返信

483件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

The C_F is related to the RC filter (or low pass filter) intended for the ADC input to have, in order to reduce the noise that will input the ADC pin.

The selection of both R_F and C_F is mainly related to the cut-off frequency that it is needed to reduce unwanted noise on the ADC input. The formula can be the one shown below:

DanielAguirre_0-1678904130217.png

Please, let us know if this information was helpful or not.

0 件の賞賛
返信