Hello, guys!
Now i 'm trying to do lpspi communication on s32k148q176 EVB. I meet some problems.
I want to use one lpspi as Master,and two lpspi as Slave. so I find one example project "lpspi_dma_s32k148". This example project can do spi communcation successfully, lpspi0 acts as Master to send data, and lpspi1 acts as Slave to receive data. Then I change its configuration. I add one CHIP SELECT pin in lpspi0 “Component Inspector->Properties->Configurations”,also add another lpspi namely lpspi2 as Slave. I try to generate code, it shows many errors. I don't know how to solve it.TAT
Here is my lpspi0-Master Configuration.
Here is lpspi1 Configuration.
Here is lpspi2 Configuration.
Here is lpspi pin Configuration.
Here are errors.
Thanks.
Liu.
Hi,
Please restart S32DS, it will work afterwards.
Thanks,
Rares