S32K146 lockup reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K146 lockup reset

1,345 Views
ivyxx
Contributor II

Dear all,

My target chip is S32K146.

I found sometime the chip resets. The RCM-SSRS code is 0X200. I read the reference manual, this reset is generated by ARM core lockup.

I have few questions on it:

1. Normally what is the reason of the lockup reset?

2. Why the system reset instead of stuck in lockup?

3. How to trace the fault? Is it possible the fault coming from hardware? I added trace code in hardfault handler and NMI handler. But nothing printed when lockup reset happened.

4. I config the NMI_b pin as I2C. Do I need to disable NMI_b interrupt by configing FTFC_FOPT?

0 Kudos
Reply
1 Reply

1,329 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) Please refer to Cortex -M4 Devices Generic User Guide

https://developer.arm.com/documentation/dui0553/latest/

 

"The processor enters a lockup state if a fault occurs when executing the NMI or HardFault handlers."

So it could be because a fault exception is detected but the fault execption handler is not implemented.

Do you have HardFault handler in the source code?

 

2) See device’s RM, section 25.2.2.8 Lockup reset (LOCKUP):

The LOCKUP gives immediate indication of seriously errant kernel software. This is the

result of the core being locked because of an unrecoverable exception following the

activation of the processor’s built in system state protection hardware.

The LOCKUP condition causes a system reset and also causes the MCU to write 1 to

RCM_SRS[LOCKUP] field.

 

3) I guess that possibly following overview could help you:

https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447

 

4) Certainly yes, I would recommend to do it so.

0 Kudos
Reply