S32K146_0N73V rev15 Errata ERR051629: LPUART:Transmit Complete bit (STAT[TC]) is not set.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K146_0N73V rev15 Errata ERR051629: LPUART:Transmit Complete bit (STAT[TC]) is not set.

401 次查看
PeiPei0416
Contributor I

Hello NXP support,

I'm checking errata on the S32K146 as follows:

PeiPei0416_0-1718590317076.png

For “Workaround”, is there any code sample? I have tried to find the workaround implementation in RTD package (RTD_4.4_R21-11_2.0.0_D2308), but I failed. The workaround is not going to be part of this RTD package.

Can you please share code sample in which the workaround is implemented?

Thank you for your support!

#S32K146

0 项奖励
回复
3 回复数

351 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @PeiPei0416 

CTS feature is not implemented in the RTD, so no workaround is needed in the RTD.

Sorry but we do not have such sample code.

Regards,

Lukas

0 项奖励
回复

321 次查看
PeiPei0416
Contributor I

Hello Lukas,

I actually emailed NXP tech support earlier and he said I could request sample code on this forum. I'd still like NXP tech support to provide sample code if possible. Thanks a lot!

Capture.PNG

0 项奖励
回复

364 次查看
PeiPei0416
Contributor I
Can anyone help?
0 项奖励
回复