S32DS组件配置问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS组件配置问题

207 Views
Ray_Tian6
Contributor I

我使用S32DS新建组件配置工程后,提示“工程中检测到的处理器内核 'ARM Bare-Metal 32-bit Target Binary Toolchain' 与当前指定的 `S32K144` 不匹配。 目标处理器不被支持或电脑不在线。”是什么原因?如何修改?

0 Kudos
Reply
1 Reply

173 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

请问你使用的S32DS和SDK是哪个版本? 建议看一下S32DS for ARM IDE v2.2与v2018.R1的差异和应用工程升级注意事项1.1 集成工具链(toolchain)的功能特性差异章节。


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply