S32K144 LSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 LSPI

4,784 Views
oceansea
Contributor III

HI,

i  use  the  LPSPI_s32k144  example,i have a question.

pastedImage_1.png

if do this is ok,no problem

but if i do this 

pastedImage_2.png

pastedImage_3.png

is inly send message ,not receive ,when counter=10,it will stop ,not run .

i only need send message,and not any slave send to me ,so my receive buff not

any message ,why it  stop here?

and why the receive will affect the send

Labels (1)
Tags (1)
0 Kudos
Reply
6 Replies

4,550 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

In this case, you need to set CFGR1_NOSTALL.

BR, Daniel

0 Kudos
Reply

4,550 Views
oceansea
Contributor III

thanks reply ,

i look this ,and i already set LPSPI1->CFGR1 = 0x00000001;

LPSPI1->CR = 0x00000000; /* Disable module for configuration */
LPSPI1->IER = 0x00000000; /* Interrupts not used */
LPSPI1->DER = 0x00000000; /* DMA not used */
LPSPI1->CFGR0 = 0x00000000; /* Defaults: */
/* RDM0=0: rec'd data to FIFO as normal */
/* CIRFIFO=0; Circular FIFO is disabled */
/* HRSEL, HRPOL, HREN=0: Host request disabled */
LPSPI1->CFGR1 = 0x00000001; /* Configurations: master mode*/
/* PCSCFG=0: PCS[3:2] are enabled */
/* OUTCFG=0: Output data retains last value when CS negated */
/* PINCFG=0: SIN is input, SOUT is output */
/* MATCFG=0: Match disabled */
/* PCSPOL=0: PCS is active low */
/* NOSTALL=0: Stall if Tx FIFO empty or Rx FIFO full */
/* AUTOPCS=0: does not apply for master mode */
/* SAMPLE=0: input data sampled on SCK edge */
/* MASTER=1: Master mode */
LPSPI1->TCR = 0x5300000F; /* Transmit cmd: PCS3, 16 bits, prescale func'l clk by 4, etc*/
/* CPOL=0: SCK inactive state is low */
/* CPHA=1: Change data on SCK lead'g, capture on trail'g edge*/
/* PRESCALE=2: Functional clock divided by 2**2 = 4 */
/* PCS=3: Transfer using PCS3 */
/* LSBF=0: Data is transfered MSB first */
/* BYSW=0: Byte swap disabled */
/* CONT, CONTC=0: Continuous transfer disabled */
/* RXMSK=0: Normal transfer: rx data stored in rx FIFO */
/* TXMSK=0: Normal transfer: data loaded from tx FIFO */
/* WIDTH=0: Single bit transfer */
/* FRAMESZ=15: # bits in frame = 15+1=16 */
LPSPI1->CCR = 0x04090808; /* Clock dividers based on prescaled func'l clk of 100 nsec */
/* SCKPCS=4: SCK to PCS delay = 4+1 = 5 (500 nsec) */
/* PCSSCK=4: PCS to SCK delay = 9+1 = 10 (1 usec) */
/* DBT=8: Delay between Transfers = 8+2 = 10 (1 usec) */
/* SCKDIV=8: SCK divider =8+2 = 10 (1 usec: 1 MHz baud rate) */
LPSPI1->FCR = 0x00000003; /* RXWATER=0: Rx flags set when Rx FIFO >0 */
/* TXWATER=3: Tx flags set when Tx FIFO <= 3 */
LPSPI1->CR = 0x00000009; /* Enable module for operation */
/* DBGEN=1: module enabled in debug mode */
/* DOZEN=0: module enabled in Doze mode */
/* RST=0: Master logic not reset */
/* MEN=1: Module is enabled */

pastedImage_1.png

0 Kudos
Reply

4,550 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

I don't see the bit being set in the code.

It should be:

LPSPI1->CFGR1 = 0x00000009;

// [3] NOSTALL = 0b1

// [0] MASTER = 0b1

BR, Daniel

0 Kudos
Reply

4,550 Views
oceansea
Contributor III

hi ,

yes ,is ny bad ,and i do LPSPI1->CFGR1 = 0x00000009;   is OK

but i still have a problem ,not any salve send to me, why the receive buff have data?

0 Kudos
Reply

4,550 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The LPSPI module is always reading the MISO port even if the pin is disconnected.

The example that you were using stopped transmitting when the RX FIFO was full to prevent overflowing.

The NOSTALL bit allows transmitting even if the RX FIFO is full.

I mentioned that to point out the issue here was the RX FIFO overflow.

But you can mask the RX data TCR_RXMSK = 1.

pastedImage_2.png

BR, Daniel

0 Kudos
Reply

4,550 Views
oceansea
Contributor III

hi,

it  really   helps ,thank your  very.

haiyang

0 Kudos
Reply