S32K144 ADC collect is not correct when voltage is below 7V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 ADC collect is not correct when voltage is below 7V

Jump to solution
431 Views
547416104
Contributor III

Hello EveryOne,

 I find the ADC collect result is not correct when battery voltage is below 7V on S32k144 100pin, the test result as below:

7.6V -> 0x288

7.5V -> 0X27B

7.4V -> 0X272

7.3V -> 0X274

7.2V -> 0x275

7.1V -> 0x277

7.0V ->  0x27A

6.9V -> 0x27C

6.8V -> 0x27E

6.7V -> 0x281

6.6V -> 0x283

6.5V -> 0x286

I use SDK to config the ADC module, whether need to do other configure for ADC module, thanks

547416104_0-1673577909111.png

547416104_1-1673577929959.png

547416104_2-1673577982502.png

547416104_3-1673577990014.png

547416104_4-1673578037870.png

 

 

 

 

0 Kudos
1 Solution
411 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Can you introduce the sampling circuit? The VADIN (ADC Input voltage) to S32K1 should be between VREFL - VREFH.
Please check if VREFH changes when the battery voltage drops, and make sure that the ADC input voltage and VREFH do not change.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
412 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Can you introduce the sampling circuit? The VADIN (ADC Input voltage) to S32K1 should be between VREFL - VREFH.
Please check if VREFH changes when the battery voltage drops, and make sure that the ADC input voltage and VREFH do not change.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
388 Views
547416104
Contributor III

The issue is fixed, HW engineer check is VREFH voltage is not ok, update the IC, the issue is fixed.

Tags (1)
0 Kudos