S32K142: FlexCAN without SOSC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K142: FlexCAN without SOSC

ソリューションへジャンプ
5,213件の閲覧回数
sripav-7
Contributor III

Hello

I have a custom board with S32K142 and I did not put an external oscillator on it because it doesn't have space on it. According to this diagram in the reference manual, it is possible to run the FlexCAN module without SOSC:

pastedImage_1.png

However, when I disable SOSC and try to initialize CAN, it halts at the can initialization step:

pastedImage_4.png

I set the clock source in CAN module to PE clock and it shows that both the module and PE clocks are set to 48 MHz. The clock manager for some reason, shows this:

pastedImage_3.png

Is it possible to run CAN without an external clock? If so, How can I fix this?

Thank you,

Harsha

ラベル(1)
0 件の賞賛
返信
1 解決策
4,634件の閲覧回数
sripav-7
Contributor III

Apparently this is a known bug in the SDK. The solution was to switch the component to flexCAN and write this in the FLEXCAN_DRV_Init function:

if(((base->MCR & CAN_MCR_MDIS_MASK) >> CAN_MCR_MDIS_SHIFT) == 0U)

{

/* To enter Disable Mode requires FreezMode first */

FLEXCAN_EnterFreezeMode(base);

FLEXCAN_Disable(base);

}

#if FEATURE_CAN_HAS_PE_CLKSRC_SELECT

/* Select a source clock for the FlexCAN engine */

FLEXCAN_SelectClock(base, data->pe_clock);

#endif

The idea is it check first if the module is already in disabled mode as expected to be the peripheral after reset and if is not already disabled then to force the freeze mode and disable the CAN module.

This workaround, at this time, is not possible using the can_pal component.

元の投稿で解決策を見る

0 件の賞賛
返信
13 返答(返信)
4,634件の閲覧回数
alexandrunan
NXP Employee
NXP Employee

Hello Alexandre,

Do you have enabled the module clock for the instance of the flexcan ?!

Try to read with the debugger the MCR register of the flexcan instance, after the clock initialization and if it crashes that is the problem.

0 件の賞賛
返信
4,634件の閲覧回数
alexandrehochar
Contributor III

Hi,

Thanks for your reply.


Yes, all clocks are set but the debugger cannot read the register.
Furthermore, no frequency are specified into the clock configuration panel in PE.
Indeed, it seems like a clock issue.

After investigation, i found the wrong setting, my system clock is set at 80 MHz.

With a 48MHz clock, registers are accessible.

I don't found a maximum system clock speed in any documentation. Someone have found something about that ?

Thank,

0 件の賞賛
返信
4,634件の閲覧回数
alexandrunan
NXP Employee
NXP Employee

I have used the sys_clock set to 80Mhz for PE engine too and the flexcan worked as supposed. The PLL it uses as clock source SOSC how did you generate the SYS clock of 80Mhz ?!

0 件の賞賛
返信
4,634件の閲覧回数
alexandrehochar
Contributor III

I tried with 8MHz and 80Mhz engine clock, it's same.

Link below my clock tree.

ClockTree.png

0 件の賞賛
返信
4,634件の閲覧回数
alexandrehochar
Contributor III

Hi,

I have the same issue. When the driver try to access of MCR register, the code crash.

I tried the fix above but without effet, the code crash when base->MCR is tested.

Someone have an idea why i can't access to CAN registers. The differences with the sample code is that i work with a 80MHz clock source. (But 8MHz Engine clock).

I also use the no-FD CAN.

Thank,

0 件の賞賛
返信
4,634件の閲覧回数
sripav-7
Contributor III

It's hard to know why. In my case, that fix is working perfectly. Are you using the can_pal component or the flexcan component?

0 件の賞賛
返信
4,634件の閲覧回数
alexandrehochar
Contributor III

Hi,

Yes, i use the can_pal.

But it seems like a clock issue.

0 件の賞賛
返信
4,634件の閲覧回数
sripav-7
Contributor III

Our issues aren't really the same, then. In my case, I used the 48 MHz clock for both system and PE and the SDK wouldn't work well with that until I used the workaround.

I'm unsure why it wouldn't work with the 80 MHz clock. Can you post a screenshot of the debug view when the code crashes?

0 件の賞賛
返信
4,634件の閲覧回数
alexandrehochar
Contributor III

Of course,

Call stack,

Dummy.png

And registers,

Register.png

Thanks a lot for your help.

0 件の賞賛
返信
4,634件の閲覧回数
sripav-7
Contributor III

I looked up the errata code and found this:

pastedImage_1.png

This document is intended for MPC574XX controller and I don't think that that register exists in S32K1XX. So I don't think ERRATA_E10595 should actually be defined. I would try deleting those lines of code and see if it works.

0 件の賞賛
返信
4,635件の閲覧回数
sripav-7
Contributor III

Apparently this is a known bug in the SDK. The solution was to switch the component to flexCAN and write this in the FLEXCAN_DRV_Init function:

if(((base->MCR & CAN_MCR_MDIS_MASK) >> CAN_MCR_MDIS_SHIFT) == 0U)

{

/* To enter Disable Mode requires FreezMode first */

FLEXCAN_EnterFreezeMode(base);

FLEXCAN_Disable(base);

}

#if FEATURE_CAN_HAS_PE_CLKSRC_SELECT

/* Select a source clock for the FlexCAN engine */

FLEXCAN_SelectClock(base, data->pe_clock);

#endif

The idea is it check first if the module is already in disabled mode as expected to be the peripheral after reset and if is not already disabled then to force the freeze mode and disable the CAN module.

This workaround, at this time, is not possible using the can_pal component.

0 件の賞賛
返信
4,634件の閲覧回数
alexandrunan
NXP Employee
NXP Employee

This workaround apply to can_pal too because it uses the FLEXCAN_DRV_Init function too to initialize the can peripheral.

0 件の賞賛
返信
4,634件の閲覧回数
sripav-7
Contributor III

I tried that and it didn't seem to work. NXP said "The can_pal is a component wrapper over the FlexCAN driver, so don’t have access directly to the Peripheral Registers."

I didn't try to troubleshoot it further because it was just easier to change my component.

0 件の賞賛
返信