S32K uses PLL, can use external crystal 4M?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K uses PLL, can use external crystal 4M?

跳至解决方案
1,530 次查看
xiabin
Contributor II

I am using the S32K configuration tool, PLL use osc 4m, clock diveder = 1; Information:

warning:the result frequency must between 8m to 32m.

标记 (1)
0 项奖励
回复
1 解答
1,397 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Xia bin

Not, unfortunately, SPLL reference frequency range is Min 8MHz and max 16MHz, so, you can't use it with an osc of 4M. Sorry for the inconveniences:

https://www.nxp.com/docs/en/data-sheet/S32K1XX.pdf#page=33 

Best regards

Jorge Alcala

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,398 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Xia bin

Not, unfortunately, SPLL reference frequency range is Min 8MHz and max 16MHz, so, you can't use it with an osc of 4M. Sorry for the inconveniences:

https://www.nxp.com/docs/en/data-sheet/S32K1XX.pdf#page=33 

Best regards

Jorge Alcala

0 项奖励
回复