S32K uses PLL, can use external crystal 4M?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K uses PLL, can use external crystal 4M?

Jump to solution
1,334 Views
xiabin
Contributor II

I am using the S32K configuration tool, PLL use osc 4m, clock diveder = 1; Information:

warning:the result frequency must between 8m to 32m.

Tags (1)
0 Kudos
Reply
1 Solution
1,201 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Xia bin

Not, unfortunately, SPLL reference frequency range is Min 8MHz and max 16MHz, so, you can't use it with an osc of 4M. Sorry for the inconveniences:

https://www.nxp.com/docs/en/data-sheet/S32K1XX.pdf#page=33 

Best regards

Jorge Alcala

View solution in original post

0 Kudos
Reply
1 Reply
1,202 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Xia bin

Not, unfortunately, SPLL reference frequency range is Min 8MHz and max 16MHz, so, you can't use it with an osc of 4M. Sorry for the inconveniences:

https://www.nxp.com/docs/en/data-sheet/S32K1XX.pdf#page=33 

Best regards

Jorge Alcala

0 Kudos
Reply