I use S32 DS CT tool to generate PORT code, it will produce the following error, how to fix it. We are expecting a reply。
#define PTD10_AUTOHOLD_Ind_OUT_PIN 10u
#define PTD10_AUTOHOLD_Ind_OUT_PORT PTD_L_HALF
#define PTD11_MII_RMII_TX_CLK_PIN 11u
#define PTD11_MII_RMII_TX_CLK_PORT PTD_L_HALF
#define PTD12_MII_RMII_TX_EN_PIN12u
#define PTD12_MII_RMII_TX_EN_PORT PTD_L_HALF
#define PTD13_LIN_IN_2_PIN 13u
#define PTD13_LIN_IN_2_PORT PTD_L_HALF
#define PTD14_LIN_OUT_2_PIN 14u
#define PTD14_LIN_OUT_2_PORT PTD_L_HALF
#define PTD15_CAN_RX_4_PIN 15u
#define PTD15_CAN_RX_4_PORT PTD_L_HALF
#define PTD16_INB4_PIN 0u
#define PTD16_INB4_PORT PTD_H_HALF
#define PTD17_INA4_PIN 1u
#define PTD17_INA4_PORT PTD_H_HALF
#define PTD20_MUX_5_AN_PIN 4u
#define PTD20_MUX_5_AN_PORT PTD_H_HALF
#define PTD21_NCV7707_IS_OUT_PIN5u
#define PTD21_NCV7707_IS_OUT_PORT PTD_H_HALF
Solved! Go to Solution.
Hi jacst,
When using S32DS3.4 with S32K3 Real Time Drivers Version 1.0.0 and S32K3xx development package(3.4.1) installed, it seems no problem.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
I have updated the version of S32 DS and RTD, the problem has been solved, thanks! @Robin_Shen
Hi jacst,
When using S32DS3.4 with S32K3 Real Time Drivers Version 1.0.0 and S32K3xx development package(3.4.1) installed, it seems no problem.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
I have updated the version of S32 DS and RTD, the problem has been solved, thanks!