Running an example s32k344

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running an example s32k344

ソリューションへジャンプ
4,730件の閲覧回数
AchrafOukheir
Contributor III

Hello ,
we just recived a the RD-HVBMSCTBUN , and I installed all necessery packages/Software in the s32ds.
I installed :

SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204

SW32K3_BMS_SDK_4.4_0.9.0_updatesite_D2210

SW32K3_BMS_SL_SDK_4.4_0.9.0_DEMO_updatesite_D2210

Installation of FreeMaster FMASTERSW31.exe

com.nxp.s32ds.s32k3.sdk.freemaster.v_3.0.repository_1.0.0.202212131557

FS26_4.4_1.0.0_RTM_DS_updatesite_D2209

and in order to start do some example I chose an example of DIO-Example-S32k344 to test our board.

1) I chose it from the sdk and of course I generate and update the code from the "S32 Configuration Tool"
2) I start builiding  FLASH (Debug_FLASH) but it stop at 31% in thise phase :

Building file: ../Project_Settings/Startup_Code/system.c

AchrafOukheir_0-1687357432017.png

 

conclusion :

I dont know what is the steps : to start developing on the board , i chose to start with ``Dio_example`` just to make my first projects with the RD-HVBMSCTBUN, hoping to do the main purpose. making an hvbms.

thank you for your help.

タグ(1)
0 件の賞賛
返信
1 解決策
4,610件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Achraf,

I see you have installed the software in the S32DS 3.5. Unfortunately the HVBMS example is not compatible with the newer S32DS 3.5 version. Please download the older S32DS 3.4 version and please install it there. It is not mentioned in the installation guide, because at the time the HVBMS software example was developed, the latest S32DS version was 3.4.

https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for...

JozefKozon_0-1688363863903.png

With Best Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,691件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Achraf,

it is very difficult, if not impossible to fix such a large software bundle. Easiest and fastest would be to uninstall everything and install it again. Please download the ug763620 "HVBMS Software Installation Guide". 

JozefKozon_1-1687508630725.png

It is very important to follow the steps in the in the "Installation Guide". As the first step must be installed the S32DS IDE. Please uninstall the S32DS IDE, then install it again and please follow the procedure. If you will not follow the install order, even if you install everything, the HVBMS software bundle will not work.

https://community.nxp.com/t5/S32K/HVBMS-bring-up-example-build-problem/td-p/1650994

With Best Regards,

Jozef

0 件の賞賛
返信
4,641件の閲覧回数
AchrafOukheir
Contributor III

I did a reinstallation , I installed all of packages and softwares that I need to run the example. I succed building the DIO example. However, when I am with the HVBMS example , It didn't work , I think its the linker 

AchrafOukheir_0-1688054413491.png


as you can see .
best regards.

0 件の賞賛
返信
4,611件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Achraf,

I see you have installed the software in the S32DS 3.5. Unfortunately the HVBMS example is not compatible with the newer S32DS 3.5 version. Please download the older S32DS 3.4 version and please install it there. It is not mentioned in the installation guide, because at the time the HVBMS software example was developed, the latest S32DS version was 3.4.

https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for...

JozefKozon_0-1688363863903.png

With Best Regards,

Jozef

0 件の賞賛
返信