Hello,
Currently In our project we are using s32k312 micro, According to that micro data sheet regarding the RAM location it is showing 192kb. But in that SRAM is having 96kb and DTCM is having 64 kb.
So i would like to know who is the using the remaining size of the ram location?
What kind of data does the DTCM and ITCM memory locations stored? Is there any particular RTD's or Peripherals which are using those memory sections.
Currently for our project we are running out of SRAM location, Can we use the Memory of the DTCM for that SRAM?
解決済! 解決策の投稿を見る。
Hello Daniel,
Sorry for the late response. I am out of office for few days.
Thanks for sharing the code. I looked into that code and I understood how we can use the DTCM and ITCM memory locations.
In our project i want to use some portion of that DTCM memory for the sram memory.
SO I created a new section for the dtcm_sram in linker file and assigned the section as shown below.
.dtcm_sram_data : AT(__sram_data_rom_end)
{
. = ALIGN(4);
__dtcm_sram_data_begin__ = .;
. = ALIGN(4);
*(.ramcode)
. = ALIGN(4);
*(.data)
*(.data*)
. = ALIGN(4);
*(.mcal_data)
. = ALIGN(4);
__dtcm_sram_data_end__ = .;
} > int_dtcm_sram
__dtcm_sram_data_rom_end = __sram_data_rom_end + (__dtcm_sram_data_end__ - __dtcm_sram_data_begin__);
I am sharing the modified linker file and the project.
Can you please let me know whether the changes are proper or not? and let me know whether can I use the DTCM memory in the way I am using it right now.
Hello @vinaychitturi,
I'm out of office, I cannot test it, but I don't see any issues in that.
Regards,
Daniel
Thanks daniel for the response.
Hello @vinaychitturi,
There is 96KB of SRAM, 32KB of ITCM and 64KB of DTCM.
Have a look at the default linker file of RTD projects.
DTCM is used for the stack.
Refer to this example:
Regards,
Daniel