I need a rbf file for the S32k144 cut2 0N47T where UART0 is used instead of UART2.
Where can I get such a rbf file or is it possible to get the source code to make my one rbf file?
Hi koehlerl,
Based on my experience with S32K144 and i can confirm the RAppID_BL works with UART1 interface. I'm using the OpenSDA microUSB connector from S32K144 EVB to program the elf into flash/ram
For that you will need to flash the RBF file first (using S32DS). Have you done that ?
Best regards,
Daniel
Hi Daniel,
I use the S32K144 EVB. I have flashed the rbf file first. But I can’t connect with the RappID BL tool.
The trace window of RappID BL Tool is empty an then after timeout the Error message comes:
There are different kinds of the rbf file for the s32K144 CPU?
BR Lutz
Von: dumitru-daniel.popa
Gesendet: Donnerstag, 31. August 2017 11:07
An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>
Betreff: Re: - Re: RappID Bootloader S32K144
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: RappID Bootloader S32K144
reply from dumitru-daniel.popa<https://community.nxp.com/people/dumitru-daniel.popa?et=watches.email.thread> in S32K - View the full discussion<https://community.nxp.com/message/938696?commentID=938696&et=watches.email.thread#comment-938696>
Petr,
That's strange. I have only cut2(0N47T) and it works fine.
Best regards,
Daniel
Daniel,
after double check, and several power down/up yours is working too. Thanks.
Anyway I have bootloader version 1.6.7.35
and the RBF file included works on cut1.
BR, Petr
Hi Lutz,
the LPUART2 (pins PTD7/TX and PTD6/RX) is used with baudrate 115200bps.
BR, Petr
Hi Petr,
but with LPUART2 I can’t connect to the PC RappID BL Tool and the trace window is empty .
With the LPUART0 I get the trace see attachment. But it don’t works.
Regards Lutz
Von: PetrS
Gesendet: Donnerstag, 31. August 2017 10:21
An: Köhler, Lutz <lutz.koehler@acd-antriebstechnik.de>
Betreff: Re: - Re: RappID Bootloader S32K144
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: RappID Bootloader S32K144
reply from Petr Stancik<https://community.nxp.com/people/PetrS?et=watches.email.thread> in S32K - View the full discussion<https://community.nxp.com/message/938684?commentID=938684&et=watches.email.thread#comment-938684>