Hello there,
I have problems importing a project.I try to use the Sent receiver on the s32k144 EVB:
and get the following error:
My steps were:
1. copy the Project folder into my workspace
2. And import it (import -> General -> Existing Projects into Workspace -> Finish)
Does anyone know how to fix it?
Best regards
解決済! 解決策の投稿を見る。
Ok, I tried several times and there are alot of things happening i do not understand.
I uninstalled s32 DS and installed again with update 11.
I import the file and:
First:
this pops up. (OK)
Second:
(OK)
Third:
(Ja)
Which steps do I have to do now? Because if I debug it now, there are these Errors:
And yes I am new to this board and design studio
Best regards
Please try to import this project by using S32 Design Studio for Arm 2018.R1 – Windows/Linux
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you for your fast answer.
When I import the Project with Arm 2018.R1 it says: Program "gcc" not found in Path.
I know there are some threads about it, but i couldn't find a solution yet.
Did you take any steps before importing the Project?
Best regards
Copy the path of unzip project.
Import Existing Projects into Workspace.
Paste the path
I have installed S32DS_ARM_v2018.R1_UP11 before, it included S32 SDK S32K1xx RTM 3.0.0.
I accidentally replied to the original post with my errors.
To add this:
I forgot to mention the Generation of the Processor Expert Code, but still those errors appear:
Best regards
Please try to add Callback Name for DMA and try to modify the DMA0_IRQHandler:
Hi,
thank you very much!
I can build it now.
Best Regards