My computer recognizes my board only as BOOTLOADER

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

My computer recognizes my board only as BOOTLOADER

跳至解决方案
957 次查看
IuliaB
Contributor I

Hello! My S32K144 wont be recognized from my computer since I updated my opensda in booatloader and loaded an example application to test my board. Since then, I cant see it on my desktop just when I put it in bootloader mode

0 项奖励
回复
1 解答
927 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi IuliaB,

I don't have S32K144EVB on hand, please refer to the SDA_INFO.HTM of S32K146EVB. You can check the version of application (APPVER) :

SDA_INFO.png

 

OpenSDA Firmware (MSD & Debug)
Firmware Apps (.zip file).

The application (MSD-DEBUG-EVB-S32K144_Pemicro_v119.SDA) can be found after download it.

If the "APPVER" value="1.19", then the application of OpenSDA has been correct updated. Then it might be due to the reset signal from the S32K144 causing OpenSDA to enter Bootloader modePlease try to disconnect J107, and then plug USB cable at J7. The S32K144EVB should not Enter OpenSDA Bootloader Mode. After connect J107(P5V_SDA_PSW-P5V0) and program S32K144 with a correct project, the reset should not output low voltage anymore.

If the "APPVER" value="0", then the application of OpenSDA has not been correct updated. Please Load an OpenSDA Application again.

Get Started with the S32K144EVB Load an OpenSDA Application.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
928 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi IuliaB,

I don't have S32K144EVB on hand, please refer to the SDA_INFO.HTM of S32K146EVB. You can check the version of application (APPVER) :

SDA_INFO.png

 

OpenSDA Firmware (MSD & Debug)
Firmware Apps (.zip file).

The application (MSD-DEBUG-EVB-S32K144_Pemicro_v119.SDA) can be found after download it.

If the "APPVER" value="1.19", then the application of OpenSDA has been correct updated. Then it might be due to the reset signal from the S32K144 causing OpenSDA to enter Bootloader modePlease try to disconnect J107, and then plug USB cable at J7. The S32K144EVB should not Enter OpenSDA Bootloader Mode. After connect J107(P5V_SDA_PSW-P5V0) and program S32K144 with a correct project, the reset should not output low voltage anymore.

If the "APPVER" value="0", then the application of OpenSDA has not been correct updated. Please Load an OpenSDA Application again.

Get Started with the S32K144EVB Load an OpenSDA Application.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复