unified_bootloader_Demo_V2.0 ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unified_bootloader_Demo_V2.0 ERROR

Jump to solution
1,569 Views
minwei
Contributor I

I am trying to use the demo S32K144_CANFD_bootloader of unified_bootloader_demo_V2.0. And there are some problems.

ERROR1:

After importing it into S32 Design Studio for ARM Version 2.2, it is shown that "The project S32K144_CANFD_bootloader was created for Kibetis SDK SDK_S32K14x_12 which is not installed in this project...".

ERROR2:

And I find an solution in the community, which suggest to install S32DS_ARM_v2018.R1_UP6.zip to solve ERROR1. However, it is shown that "The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration", when the ZIP is stalling.

0 Kudos
Reply
1 Solution
1,560 Views
Senlent
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2 Replies
1,564 Views
minwei
Contributor I

By the way, I have tried to reinstall S32 Design Studio for ARM Version 2.2 in D:\NXP and C:\. However, it doesn't work.

0 Kudos
Reply
1,561 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@minwei

please try install the IDE in the picture below, and install SDK_S32K14X_12

https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for... 

Senlent_1-1661912571752.png

 

0 Kudos
Reply