MCU restarting when controlling a motor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCU restarting when controlling a motor

1,786 次查看
elb1
Contributor III

Hello, i am using s32k142 microcontroller, and when i am controlling a motor (pwm, direction) the applicxation will be restarted all the time, and when i have seen the RCM register to know the reason for reset, LOCKUP bit is set, but what can be the cause for this 
Thank you in advance.

0 项奖励
回复
10 回复数

1,644 次查看
elb1
Contributor III

Hello Daniel, 
Now it goes to one of the handlers, and it is actually going to "HardFault_Handler", but there is no much information about it in the link you sent me, do you have any idea what "HardFault_Handler" means, or what can be the problem ?
Thank you

0 项奖励
回复

1,626 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @elb1,

This is explained in the document, and the example handles hard faults too:

https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447

 

BR, Daniel

0 项奖励
回复

1,764 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @elb1,

When the core detects a fault exception, it fetches the HardFault_Hander().

The exception is then escalated to Core Lockup if the core detects another exception during the fetching.

Therefore I would say there is no HardFault_Hander() in the project.

Refer to this document/example, you should be able to find the exception that causes the fault.

https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447

 

Regards,

Daniel

0 项奖励
回复

1,758 次查看
elb1
Contributor III

Hello Daniel, Thank you for your response.
I have added those fault_exception files and it worked fine the microcontroller is not reset and also the control of the motor is working perfectly.
But the problem is that i didn't do anything except adding handlers, so is the problem still there ? or i don't know, i have also put break points in all those handlers but it didn't went to anyone of them

Thank you

0 项奖励
回复

1,753 次查看
elb1
Contributor III

Hello, more updates:
it was working only when i have put application only (in debug mode), but when flashed it with bootloader i got again the same behavior, the mcu is restarting and the reason again is LOCKUP, it also didn't stop in any of the handlers, it will be stopped somewhere in
No source available for "0x7bcce0e6" 

0 项奖励
回复

1,725 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @elb1,

ARM documentation states:

"The processor enters a lockup state if a fault occurs when executing the NMI or HardFault handlers."

https://developer.arm.com/documentation/dui0646/c/The-Cortex-M7-Processor/Fault-handling/Lockup?lang...

It could be because the HardFault vector is not implemented, therefore, I recommended adding it to the project.

Regarding the bootloader, please make sure the VTOR address is correctly changed to the vector table of the application. And read the HardFault vector in the memory view to ensure it has the pointer to the handler.

 

Regards,

Daniel

 

0 项奖励
回复

1,719 次查看
elb1
Contributor III

Hello Daniel, thank you for your response,
The thing is even when i divide for example by zero, to see if one of the handlers will be triggered but nothing, i think i am not testing as i should. I also tested with example project that you have provided you take a look at my response, i have put a comment there. 

https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447 

Thank you so much, i appreciate your help

0 项奖励
回复

1,687 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @elb1,

I just replied to your comment there.

Can you test the division by 0 in a new empty project?

Don't forget to enable the division by 0 trap.

 

Can you attach your project here so that I can test it?

 

BR, Daniel

0 项奖励
回复

1,681 次查看
elb1
Contributor III

Hi, yes i have enabled the division by 0 trap
I  actually have tested in hello_world project, and it is going to the "UsageFault_Handler".
It's really strange in my project it doesn't, do you have any idea why?
Ps.I am using an RTOS operating system in my project, but even if i didn't started nor initializing any task, it still doesn't go to the handler.
Thank you

0 项奖励
回复

1,666 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Are the handlers define in the startup_S32K142.S file

Have you checked the vector table in the flash?

Does it point to the handlers?

Can you share the project?

 

Regards,

Daniel

0 项奖励
回复