MCSPTE1AK344

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCSPTE1AK344

467件の閲覧回数
Canberk
Contributor II

 

I already have DEVKIT-MOTORGD and S32K344. I wanna use them as MCSPTE1AK344. İs the possible to work with it just like MCSPTE1AK344

Thanks

0 件の賞賛
返信
2 返答(返信)

460件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

It is possible to use it, but there are thing which need to be clarified.

1. which S32K344 board you mean.

2. there are done modification to resistors on board in NXP fab for MOTOR-GD kit. This also depends on board revision A or B.

Best regards,

Peter

 

0 件の賞賛
返信

459件の閲覧回数
Canberk
Contributor II

Thanks for answering.

this is the board I talked about:

S32K3x4-Q172 General-Purpose Development Board | NXP Semiconductors

and I have got MOTOR-GD kit from MCSPTE1AK144 S32K144 BLDC/PMSM Development Kit | NXP Semiconductors

@petervlna 

 

0 件の賞賛
返信