MCSPTE1AK344

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCSPTE1AK344

464 Views
Canberk
Contributor II

 

I already have DEVKIT-MOTORGD and S32K344. I wanna use them as MCSPTE1AK344. İs the possible to work with it just like MCSPTE1AK344

Thanks

0 Kudos
Reply
2 Replies

457 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

It is possible to use it, but there are thing which need to be clarified.

1. which S32K344 board you mean.

2. there are done modification to resistors on board in NXP fab for MOTOR-GD kit. This also depends on board revision A or B.

Best regards,

Peter

 

0 Kudos
Reply

456 Views
Canberk
Contributor II

Thanks for answering.

this is the board I talked about:

S32K3x4-Q172 General-Purpose Development Board | NXP Semiconductors

and I have got MOTOR-GD kit from MCSPTE1AK144 S32K144 BLDC/PMSM Development Kit | NXP Semiconductors

@petervlna 

 

0 Kudos
Reply