Hi ,
I'm using TCP/IP demo example from SW32K3_TCPIP_RTM_1_0_1_HF1_D2209 on evaluation board - S32K3X4EVB-Q172
Before running the example , I have closed J18:2-3 on S32K3X4EVB-Q172 board, as mentioned in example's description.txt file
I have setup the Host PC with static IP address 192.168.0.100/255.255.255.0 and trying to run pin command . But it never gets reply from S32K3X4EVB-Q172 (which is configure with IP address 192.168.0.200). When I debug the code , I can see that board can receive the packets but cannot parse it.
For example, When I debug function Gmac_Ip_ReadFrame() from file Gmac_Ip.c , ethernet packets header is parsed , but some how PayloadType is showing GMAC_IP_PAYLOAD_TYPE_UNKNOWN. (Please refer attached file.)
Below is my SW tools version details :
S32K344 RTD version
o S32 Design Studio 3.5
o SW32K3_TCPIP_RTM_1_0_1_HF1_D2209
o S32K3 RTD RTM 2.0.1 integration layer
o S32K3 FreeRTOS 10.4.6 version 2.0.1
In my understanding , this default example should work without any change. May be I am missing some configuration.
Please help to resolve this issue.
Regards,
Sanjay
Hi @JRoberto,
Thanks for your reply. S32K3X4EVB-Q172 EVK board , I am using has Texas Instruments DP83848C phy chip.
We have tried both version RDT 2.0.1 and RTD 2.0.0 , it's same behavior. Anyways, let me double check with RTD 2.0.0 and get back to you.
Appreciate your attention to this thread!
Regards,
Sanjay
Hello @sanjaytandel
Could you please tell me which ethernet transceiver does your board has soldered? It's the IC highlighted in the picture
Also, I noticed that you have the RTD 2.0.1 but it may cause troubles... could you try using the recommended software for RTM 2.0.0?
Best Regards!