LDF LIN stack generate lin cfg code miss

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LDF LIN stack generate lin cfg code miss

跳至解决方案
1,507 次查看
liuxing_hu
Contributor III

liuxing_hu_0-1629855169086.png

as the picture show, there are 2 slave frames(LIN_Slave_SWSR_SWIT and LIN_Slave_SWSL_SWIT) in LDF file, but when reload LDF file, and generate, only the code of LIN_Slave_SWSL_SWIT  generate in lin_cfg.h, I can'r find the code of LIN_Slave_SWSR_SWIT in lin_cfg.h, does I miss something to config?

0 项奖励
回复
1 解答
1,493 次查看
hungnguyenphi
NXP Employee
NXP Employee

Hello @liuxing_hu ,

 

One interface in the MCU will represent just one node in the Lin Network which is described in the LDF file. Then the LinStack just generated the code for the corresponding node.

hungnguyenphi_1-1629968334568.png

 

Best regards,

Hung

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,392 次查看
gaowei
Contributor I

我的S32DS 出现lin ldf文件不能用通过Generated方式输出内容到lin_cfg.c 和.H. ;lin_cfg.c文件中内容没有ldf的相关内容。请问您觉得可能是哪里出了问题?

0 项奖励
回复
1,494 次查看
hungnguyenphi
NXP Employee
NXP Employee

Hello @liuxing_hu ,

 

One interface in the MCU will represent just one node in the Lin Network which is described in the LDF file. Then the LinStack just generated the code for the corresponding node.

hungnguyenphi_1-1629968334568.png

 

Best regards,

Hung

0 项奖励
回复