Interrupt api is not called in case of SMR Verification is Periodic in S32K3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupt api is not called in case of SMR Verification is Periodic in S32K3

Jump to solution
1,782 Views
HyunungPark1
Contributor III

Hi.

Interrupt api is not called in case of SMR Verification is Periodic in S32K3.

Could you please let me know why Interrupt api is not called?

0 Kudos
1 Solution
1,277 Views
nxf78987
NXP Employee
NXP Employee

Hello @HyunungPark1,

Sorry for my late response.

Did you check the below bits in your program?

NVIC->ISER6 bit 4: Set if you enabled MU0 interrupt.
NVIC->IABR6 bit 4: Set if iMU0 interrupt occurred.
 
Best regards,
Dan

View solution in original post

0 Kudos
12 Replies
1,716 Views
nxf78987
NXP Employee
NXP Employee

Hello @HyunungPark1,

Could you send me the code implemented in the CDD_InitFTDConfiguration() function and Fls configuration?

And what is the HSE Firmware you are using?

Best regards,

Dan

0 Kudos
1,677 Views
HyunungPark1
Contributor III

Hi.

below is the information for RTD and HSE Firmware which  I used

RTD : SW32K3_RTD_4.4_R21-11_3.0.0_P01_HF02
 
HSE FW : s32k3x4_hse_fw_0.5.0_2.1.0_pb220625.bin.pink
 
and below is the procedure and code for smr verifiation - peridoc 
 
============ CDD_InitFTDConfiguration ============= 
 
#define RSA_TAG_FTD_SIGNATURE_FLASH_ADDRESS 0x10000400UL
 
g_smrEntry[smrIndex].configFlags = HSE_SMR_CFG_FLAG_QSPI_FLASH ;
g_smrEntry[smrIndex].pSmrDest = 0x20430000;
g_smrEntry[smrIndex].checkPeriod = 100;
g_smrEntry[smrIndex].pSmrsrc=0x0046c000;
g_smrEntry[smrIndex].smrSize = 256;
g_smrEntry[smrIndex].authKeyHandle = CRYPTO_KEY_ID_NVM_FTD_PUBLICKEY_HANDLE;
g_smrEntry[smrIndex].authScheme.sigScheme.signSch = HSE_SIGN_RSASSA_PKCS1_V15;
g_smrEntry[smrIndex].authScheme.sigScheme.sch.rsaPkcs1v15.hashAlgo = HSE_HASH_ALGO_SHA2_256;
g_smrEntry[smrIndex].pInstAuthTag[0] = RSA_TAG_FTD_SIGNATURE_FLASH_ADDRESS; 
g_smrEntry[smrIndex].pInstAuthTag[1] = (uint32_t)NULL;
 
============ the procedure ============= 
1. IntCtrl_Ip_InstallHandler(HSE_MU0_ORED_IRQn, &Mu_Ip_Mu0_OredGP_Isr, NULL_PTR); 
    -> Install ORed GP interrupt for MU-0
 
2. IntCtrl_Ip_EnableIrq(HSE_MU0_ORED_IRQn) 
    -> Enable ORed GP interrupt for MU-0
 
3. Hse_Ip_RegisterGenericCallback(Crypto_aPartitionToMuMapping[0].u8MuInstance, u32NotifEventsMask, GenericPurposeCallback)
   -> Registers a general purpose callback
 
4.  Status   = CDD_InitSBConfiguration(...)
   -> Set configuration for SMR Verification-Boot
 
5. Status = CDD_InitFTDConfiguration(...)
   -> Set configuration for SMR Verification - Periodic
 
6.  Reset Device
 
7.  Change the firmware using Fls_Erase and Fls_Write ap
 
==> The below is not called
     ISR(Mu_Ip_Mu0_OredGP_Isr)
     {
     Hse_Ip_GeneralPurposeIrqHandler(0U);
      }
 
BRs.
Hyunung Park
0 Kudos
1,702 Views
HyunungPark1
Contributor III

Hi.

below is the information for RTD and HSE Firmware which  I used

RTD : SW32K3_RTD_4.4_R21-11_3.0.0_P01_HF02
 
HSE FW : s32k3x4_hse_fw_0.5.0_2.1.0_pb220625.bin.pink
 
and below is the procedure and code for smr verifiation - peridoc 
 
============ CDD_InitFTDConfiguration ============= 
 
#define RSA_TAG_FTD_SIGNATURE_FLASH_ADDRESS 0x10000400UL
 
g_smrEntry[smrIndex].configFlags = HSE_SMR_CFG_FLAG_QSPI_FLASH ;
g_smrEntry[smrIndex].pSmrDest = 0x20430000;
g_smrEntry[smrIndex].checkPeriod = 100;
g_smrEntry[smrIndex].pSmrsrc=0x0046c000;
g_smrEntry[smrIndex].smrSize = 256;
g_smrEntry[smrIndex].authKeyHandle = CRYPTO_KEY_ID_NVM_FTD_PUBLICKEY_HANDLE;
g_smrEntry[smrIndex].authScheme.sigScheme.signSch = HSE_SIGN_RSASSA_PKCS1_V15;
g_smrEntry[smrIndex].authScheme.sigScheme.sch.rsaPkcs1v15.hashAlgo = HSE_HASH_ALGO_SHA2_256;
g_smrEntry[smrIndex].pInstAuthTag[0] = RSA_TAG_FTD_SIGNATURE_FLASH_ADDRESS; 
g_smrEntry[smrIndex].pInstAuthTag[1] = (uint32_t)NULL;
 
============ the procedure ============= 
1. IntCtrl_Ip_InstallHandler(HSE_MU0_ORED_IRQn, &Mu_Ip_Mu0_OredGP_Isr, NULL_PTR); 
    -> Install ORed GP interrupt for MU-0
 
2. IntCtrl_Ip_EnableIrq(HSE_MU0_ORED_IRQn) 
    -> Enable ORed GP interrupt for MU-0
 
3. Hse_Ip_RegisterGenericCallback(Crypto_aPartitionToMuMapping[0].u8MuInstance, u32NotifEventsMask, GenericPurposeCallback)
   -> Registers a general purpose callback
 
4.  Status   = CDD_InitSBConfiguration(...)
   -> Set configuration for SMR Verification-Boot
 
5. Status = CDD_InitFTDConfiguration(...)
   -> Set configuration for SMR Verification - Periodic
 
6.  Reset Device
 
7.  Change the firmware using Fls_Erase and Fls_Write ap
 
==> The below is not called
     ISR(Mu_Ip_Mu0_OredGP_Isr)
     {
     Hse_Ip_GeneralPurposeIrqHandler(0U);
      }
 
BRs.
Hyunung Park
0 Kudos
1,698 Views
nxf78987
NXP Employee
NXP Employee

Hello @HyunungPark1,

I saw that you have not called "Hse_Ip_Init(MU0_INSTANCE_U8, &HseIp_MuState);" in your code to init MU_0.

So, you need to call "Hse_Ip_GetHseStatus(MU0_INSTANCE_U8);" and "Hse_Ip_Init(MU0_INSTANCE_U8, &HseIp_MuState);" after "IntCtrl_Ip_EnableIrq(HSE_MU0_ORED_IRQn);"

Best regards,

Dan

0 Kudos
1,674 Views
HyunungPark1
Contributor III
Hi
 
my code call Hse_Ip_Init like below code
 
/* Install ORed GP interrupt for MU-0 */
  IntCtrl_Ip_InstallHandler(HSE_MU0_ORED_IRQn, &Mu_Ip_Mu0_OredGP_Isr, NULL_PTR);
 
  /* Enable ORed RX interrupt for MU-0 */
  IntCtrl_Ip_EnableIrq(HSE_MU0_ORED_IRQn);
 
/* Initialize Crypto driver */
Crypto_Init(NULL_PTR); ==> Hse_Ip_Init is called by this api
 
RetVal = Crypto_GetAttribute(HSE_SECURE_LIFECYCLE_ATTR_ID,sizeof(hseAttrSecureLifecycle_t) ,(void *)&gHseCurrentLC);
 
if(RetVal == E_OK && (gHseCurrentLC & HSE_LC_CUST_DEL == HSE_LC_CUST_DEL)){
RetVal = CDD_CheckKeyProvisioning();
if(RetVal == E_NOT_OK){
/* Format HSE key catalogs (RAM + NVM) */
RetVal = Crypto_Exts_FormatKeyCatalogs();
//CDDAssert((Std_ReturnType)E_OK == RetVal);
}else{
}
}else{
RetVal = E_OK;
}
Hse_Ip_RegisterGenericCallback(Crypto_aPartitionToMuMapping[0].u8MuInstance, u32NotifEventsMask, GenericPurposeCallback);
return RetVal;
 
BRs.
Hyunung Park
0 Kudos
1,652 Views
HyunungPark1
Contributor III

Hi

This issue is not resoived.

Hyunung Park

0 Kudos
1,593 Views
nxf78987
NXP Employee
NXP Employee

Hello @HyunungPark1,

I have a question: when you perform step 6 (Reset Device) then after that: Is your program run step 1 to 5 again?

Best regards,

Dan

 

0 Kudos
1,579 Views
HyunungPark1
Contributor III

Hello Dan

My program doesn't run step 1 to 5 again after step 6 (Reset Device) 

Best Regards.

Hyunung Park

0 Kudos
1,573 Views
nxf78987
NXP Employee
NXP Employee

Hello @HyunungPark1,

If your program doesn't run step 1 to 5 again after step 6 (Reset Device) then it mean the value of registers was reset and indicated that HSE_MU0_ORED interrupt was not enable when you perform test.

Best regards,

Dan

0 Kudos
1,569 Views
HyunungPark1
Contributor III

Hello Dan.

I think that HSE_MU0_ORED interrupt is enable because the below code is performed after device reset

/* Install ORed GP interrupt for MU-0 */
IntCtrl_Ip_InstallHandler(HSE_MU0_ORED_IRQn, &Mu_Ip_Mu0_OredGP_Isr, NULL_PTR);

/* Enable ORed RX interrupt for MU-0 */
IntCtrl_Ip_EnableIrq(HSE_MU0_ORED_IRQn);

Best Regards.

Hyunung Park

0 Kudos
1,278 Views
nxf78987
NXP Employee
NXP Employee

Hello @HyunungPark1,

Sorry for my late response.

Did you check the below bits in your program?

NVIC->ISER6 bit 4: Set if you enabled MU0 interrupt.
NVIC->IABR6 bit 4: Set if iMU0 interrupt occurred.
 
Best regards,
Dan
0 Kudos
1,191 Views
HyunungPark1
Contributor III

Hi.

This issue is resloved.

Hyunung Park