Input PWM is zero for SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Input PWM is zero for SDK

跳至解决方案
5,674 次查看
linglei_meng
Contributor II

Hello Community

We want to detect the Crash signal input and configure it according to the example, but there is no return value of IC_GETMEASUREMENT (), please help us to check whether we made a mistake in the configuration.

 

Chip version:S32K148 -> 144

PIN: PTD18  

Hardware environment: SRS analog input
Config: FTM5_CH7

for example: ic_pal_s32k148

MCU detects CRASH signal input,

 

 


uint16_t inputCaptureMeas = 0U;
uint16_t inputMeas = 0U;
uint32_t frequency;
uint8_t channel = ic_pal1_ChnConfig->hwChannelId;

IC_Init(&ic_pal1_instance, &ic_pal1_InitConfig);

while(1)
{
    frequency = FTM_DRV_GetFrequency(ic_pal1_instance.instIdx);
    inputCaptureMeas = IC_GetMeasurement(&ic_pal1_instance, channel);
    inputMeas = frequency / (inputCaptureMeas);

    JPCC_DEBUG(JPCC_LOG_LEVEL_WARNING, "[ SensorApp] 6 PWM uFrequencyHZ=[%lu],         frequency=[%lu], inputCaptureMeas=[%u], inputMeas=[%lu]\r\n",
    flexTimer_pwm1_PwmConfig.uFrequencyHZ, frequency, inputCaptureMeas, inputMeas);

    OS_sleep(300);
};

 

 

 

 

0 项奖励
1 解答
5,489 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Looking at the screenshots you posted, I see the FTM frequency is set to 256Hz.

The resolution is therefore 1/256 = 3.9ms

3.9ms * 28 = 109.2ms which is 91% of 120ms.

If you need to have a higher resolution, you need to set a higher FTM frequency.

 

Regards,

Daniel

 

 

在原帖中查看解决方案

9 回复数
5,572 次查看
linglei_meng
Contributor II
 
 
 
 
 
 

  The signal input frequency we use is as shown in "crah.jpg",I don't know how to calculate the duty cycle according to them. Could you please give me a calculation method or formula?

0 项奖励
5,605 次查看
linglei_meng
Contributor II

Configuration changes

PIN: PTC10

Hardware environment: SRS analog input
Config: FTM3_CH4

The current configuration has SRS input.

We would like to know how to calculate the duty cycle. Could you provide a specific calculation formula?

 

6148 = IC_GetMeasurement(&ic_pal1_instance, channel);

duty = 40%.

 

0 项奖励
5,590 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The IC_GetMeasurement() function returns the duty-cycle value in FTM3 ticks (24MHz).

If you know the period of the input signal, you can easily calculate the duty-cycle in %.

 

Regards,

Daniel

0 项奖励
5,570 次查看
linglei_meng
Contributor II

Our input signal (Type)

T = 120ms.

Hz = 0.0083333333333KHz

How do we use the data we have to calculate the duty cycle?Could you give me an example? Thank you

 

0 项奖励
5,553 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The IC_GetMeasurement() function returns number of FTM ticks measured while the input signal is ON.

One FTM tick is one period of the FTM function clock.

 

Instead of the PAL driver, you can use the FTM_IC driver.

Example: ftm_signal_measurement_s32k148

With this configuration:

danielmartynek_0-1615984207385.png

The driver can measure input signal:

danielmartynek_2-1615984291953.png

If you need to measure signal of frequency 8.33Hz, you need to select a slower FTM clock.

For example,

danielmartynek_3-1615984490380.png

danielmartynek_4-1615984521734.png

In this case, 1 FTM clock cycle = 1 FTM tick = 1/62500 = 16us is resolution of the measurement.

You could use faster FTM clock frequency but you would need to count the FTM overflows and add it to the time captured between the two edges.

 

Regards,

Daniel

 

 

 

0 项奖励
5,499 次查看
linglei_meng
Contributor II

Our input signal (Type)

T = 120ms.

Hz = 0.0083333333333KHz

Duty = 90%

FTM_DRV_GetInputCaptureMeasurement(INST_FLEXTIMER_IC1, 4U)  = 28;

1 FTM clock cycle = 1 FTM tick = 1/62500 = 16us is resolution of the measurement.

Duty cycle calculation formula:  (28 * 16us) / 120ms = 90%  

Is that the calculation?

Could you specify the duty cycle calculation formula with the above parameters.

linglei_meng_4-1617011154697.png

 

linglei_meng_1-1617010768244.pnglinglei_meng_2-1617010944153.pnglinglei_meng_3-1617011010840.png

 

 

 

0 项奖励
5,490 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Looking at the screenshots you posted, I see the FTM frequency is set to 256Hz.

The resolution is therefore 1/256 = 3.9ms

3.9ms * 28 = 109.2ms which is 91% of 120ms.

If you need to have a higher resolution, you need to set a higher FTM frequency.

 

Regards,

Daniel

 

 

5,644 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Could you please attach the project?

The issue could be in the PIN driver, for example.

Can you scope the signal on PTD18?

 

Thank you,

BR, Daniel

0 项奖励
5,667 次查看
linglei_meng
Contributor II

Analog CRASH signal

0 项奖励