I used S32K344,
IDE is S32DS3.4 ,
RTD is S32K3 RTD AUTOSAR 4.4 VERSION 2.0.0
I Set S32K344 in SOC_STANDBY mode by Power_Ip_SetMode(soc_standby), and I Found the current consumption is 14mA, the request is less 3 mA.
what step I lost? like deinitial some mode used? or switch clock to FISR? I tried so many but not worked!
I wish there is example project to learn it, Hope to get your help, thanks.
已解决! 转到解答。
Thanks you very much.
I find out my problem. there are two pin config as SPI_OUT which increase current consumption in SOC_STANDBY mode. So I config those 2 pin as GPIO_OUT_LOW before enter SOC_STANDBY mode. and the problem is solved!
Thanks you very much.
I find out my problem. there are two pin config as SPI_OUT which increase current consumption in SOC_STANDBY mode. So I config those 2 pin as GPIO_OUT_LOW before enter SOC_STANDBY mode. and the problem is solved!