How to lower the CPU frequency of the S32K314?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to lower the CPU frequency of the S32K314?

ソリューションへジャンプ
339件の閲覧回数
gumu
Contributor IV

Dear Sir,

We have a requirement in our project to change the CPU operating frequency of the S32K314 from the original 160MHz to 100MHz. Where can we make this change? Additionally, what are the impacts of reducing the CPU frequency?

Thanks!

0 件の賞賛
返信
1 解決策
307件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

You can use multiple clock configuration in the S32DS.

davidtosenovjan_0-1716297397434.png

It is needed to keep clocking options as defined in device's RM

Table 145. System clocking configurations

davidtosenovjan_1-1716297554200.png

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
308件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

You can use multiple clock configuration in the S32DS.

davidtosenovjan_0-1716297397434.png

It is needed to keep clocking options as defined in device's RM

Table 145. System clocking configurations

davidtosenovjan_1-1716297554200.png

 

 

 

0 件の賞賛
返信