s32k144-q100 autosar mcal with EB tresos hello world

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k144-q100 autosar mcal with EB tresos hello world

193 Views
spara7c5
Contributor III

Hello community,
I would build and run a basic blink led  s32k144-q100 EVB with autosar stack.
HW setup:

  • s32k144-q100 EVB

SW setup:

  • EB tresos S32Kxx version
  • S32DS with S32Kxx plugin + S32K1XX_sMCAL_4.2_RTM_1.0.6

Current status:

  • successfully tried the build+flash+debug of the example blinkLED with S32DS
  • successfully genretaed Autosar code with EB tresos for demo "simple_demo_rte"

Now, how can i intregrate the generated autosar code to a S32DS project and compile+run+debug?

Thanks in advance,
Stefano

0 Kudos
1 Reply

85 Views
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
I afraid you have to upgrade your AUTOSAR version to 4.4 or 4.7.
S32DS doesn't support MCAL 4.2.
If you want to use S32DS, I refer you to install Real Time Driver product that available in NXP.com site. 

cuongnguyenphu_0-1716290060343.png


In Realtime Driver (RTD) product we provided example for each MCAL module, also have Dio example with blinks LED 

cuongnguyenphu_1-1716290220751.png

 

 

 

0 Kudos