How to lower the CPU frequency of the S32K314?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to lower the CPU frequency of the S32K314?

Jump to solution
166 Views
gumu
Contributor IV

Dear Sir,

We have a requirement in our project to change the CPU operating frequency of the S32K314 from the original 160MHz to 100MHz. Where can we make this change? Additionally, what are the impacts of reducing the CPU frequency?

Thanks!

0 Kudos
Reply
1 Solution
134 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

You can use multiple clock configuration in the S32DS.

davidtosenovjan_0-1716297397434.png

It is needed to keep clocking options as defined in device's RM

Table 145. System clocking configurations

davidtosenovjan_1-1716297554200.png

 

 

 

View solution in original post

0 Kudos
Reply
1 Reply
135 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

You can use multiple clock configuration in the S32DS.

davidtosenovjan_0-1716297397434.png

It is needed to keep clocking options as defined in device's RM

Table 145. System clocking configurations

davidtosenovjan_1-1716297554200.png

 

 

 

0 Kudos
Reply