How to lower the CPU frequency of the S32K314?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to lower the CPU frequency of the S32K314?

跳至解决方案
192 次查看
gumu
Contributor IV

Dear Sir,

We have a requirement in our project to change the CPU operating frequency of the S32K314 from the original 160MHz to 100MHz. Where can we make this change? Additionally, what are the impacts of reducing the CPU frequency?

Thanks!

0 项奖励
回复
1 解答
160 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

You can use multiple clock configuration in the S32DS.

davidtosenovjan_0-1716297397434.png

It is needed to keep clocking options as defined in device's RM

Table 145. System clocking configurations

davidtosenovjan_1-1716297554200.png

 

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
161 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

You can use multiple clock configuration in the S32DS.

davidtosenovjan_0-1716297397434.png

It is needed to keep clocking options as defined in device's RM

Table 145. System clocking configurations

davidtosenovjan_1-1716297554200.png

 

 

 

0 项奖励
回复