@
Hi guys,
I have a question, ask for your help.
In the project example of ‘flash_partitioning_s32k142’ all of FlexNVM(64k) is set as EEPROM backup region, all of FlexRAM(4K) is set as EEPROM.
Could I separate half of FlexNVM as D-flash to store program, and half of FlexNVM as EEPROM backup region? also FlexRAM do not need to be configured as much as 4K to be EEPROM, only need a few bytes needed, Configure rest of FlexRAM as ram?
If convenient could you give me some reference code.
Thanks.
S32 SDK@all experts
解決済! 解決策の投稿を見る。
Hello,
I would like to suggest checking AN11983 - Using the S32K1xx EEPROM Functionality
https://www.nxp.com/docs/en/application-note/AN11983.pdf
Yes, it is possible to split FlexNVM.
The options how to split the FlexNVM block between D-Flash and emulated EEPROM backup memory (E-Flash), see below:
This setting represents "DEPartitionCode" parameter in the "FLASH_DRV_DEFlashPartition()" function
About your second question related to FlexRAM. The FlexRAM cannot be split, we can use only the whole FlexRAM as an SRAM or EEPROM.
I hope it helps.
Best regards,
Diana
Hello,
I would like to suggest checking AN11983 - Using the S32K1xx EEPROM Functionality
https://www.nxp.com/docs/en/application-note/AN11983.pdf
Yes, it is possible to split FlexNVM.
The options how to split the FlexNVM block between D-Flash and emulated EEPROM backup memory (E-Flash), see below:
This setting represents "DEPartitionCode" parameter in the "FLASH_DRV_DEFlashPartition()" function
About your second question related to FlexRAM. The FlexRAM cannot be split, we can use only the whole FlexRAM as an SRAM or EEPROM.
I hope it helps.
Best regards,
Diana
it works! thanks
When the partition code is not set to full data flash, the data set size can be set to any of several non-zero values dqfansurvey.