Hello NXP team,
we are developing bootloader for S32K314 and we'd like to know how to get bootloader example?
Thanks!
Solved! Go to Solution.
please taka a look at this post,
https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099
please taka a look at this post,
https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099
Hello,Sir!This attachment is my s32k312 bootloader&app project,but it cannot run properly!Could you help me take a look at how to modify this code,please! Also, the Unified Bootloader Demo is looks at difficult. Can you provide me with a simpler example?
/* bootloader_linker */
MEMORY
{
int_flash : ORIGIN = 0x00400000, LENGTH = 0x00010000 /* 2048K - 176K (sBAF + HSE)*/
int_itcm : ORIGIN = 0x00000000, LENGTH = 0x00008000 /* 32K */
int_dtcm : ORIGIN = 0x20000000, LENGTH = 0x00010000 /* 64K */
int_sram : ORIGIN = 0x20400000, LENGTH = 0x00006F00 /* 27 KB */
int_sram_fls_rsv : ORIGIN = 0x20406F00, LENGTH = 0x00000100
int_sram_stack_c0 : ORIGIN = 0x20407000, LENGTH = 0x00001000
int_sram_no_cacheable : ORIGIN = 0x20408000, LENGTH = 0x00007F00 /* 32kb , needs to include int_results */
int_sram_results : ORIGIN = 0x2040FF00, LENGTH = 0x00000100
int_sram_shareable : ORIGIN = 0x20410000, LENGTH = 0x00008000 /* 32KB */
ram_rsvd2 : ORIGIN = 0x20418000, LENGTH = 0 /* End of SRAM */
}
/*bootloader_main.c*/
/* ========== define var ========== */
#define APP_START_ADDRESS (0x000410000 + 0x200) //app开始地址
/*=========== LOCAL FUNCTIONS =========*/
void Bootup_Application(const uint32_t app_StarAddress);
void init_ram(void);
void TestDelay(uint32 delay);
void TestDelay(uint32 delay)
{
static volatile uint32 DelayTimer = 0;
while (DelayTimer<delay)
{
DelayTimer++;
}
DelayTimer=0;
}
/**
* @brief Main function of the example
* @details Initializez the used drivers and uses the Icu
* and Dio drivers to toggle a LED on a push button
*/
int main(void)
{
uint8 count = 0U;
/* Initialize all pins using the Port driver */
Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);
while (count++ < 5)
{
Siul2_Dio_Ip_WritePin(LED_PORT, LED_PIN, 1U);
TestDelay(4800000);
Siul2_Dio_Ip_WritePin(LED_PORT, LED_PIN, 0U);
TestDelay(4800000);
}
/* 清空ECC */
init_ram();
/* 执行跳转 */
Bootup_Application(APP_START_ADDRESS);
return (0U);
}
#define STDBYRAM_START 0x20400000
#define STDBYRAM_END 0x20418000
#define STDBYRAM_SIZE (STDBYRAM_END - STDBYRAM_START)
void init_ram(void)
{
uint32_t cnt;
uint64_t *pDest;
cnt = (( uint32_t)(STDBYRAM_SIZE)) / 8U;
pDest = (uint64_t *)(STDBYRAM_START);
while (cnt--)
{
*pDest = (uint64_t)0x00;
pDest++;
}
}
/*
* start_Bootup_Application
* */
void Bootup_Application(const uint32_t app_StarAddress)
{
uint32_t appEntry, appStack;
static void (*jump_to_application)(void);
/* 获取栈地址 */
appStack = *((uint32_t *)(app_StarAddress));
/* 获取app入口地址 */
appEntry = *((uint32_t *)(app_StarAddress + 4));
/*把应用程序入口地址赋值给函数指针*/
jump_to_application = (void (*)(void))appEntry;
/* 重新定向中断向量表 */
S32_SCB->VTOR = (uint32_t)app_StarAddress;
/* 关闭全局中断 ASM_KEYWORD("cpsid i"); */
__asm volatile ("cpsid i" : : : "memory");
/* 设置栈指针 */
__asm volatile ("MSR msp, %0\n" : : "r" (appStack) : "memory");
__asm volatile ("MSR psp, %0\n" : : "r" (appStack) : "memory");
/*跳转*/
jump_to_application();
while (1)
{
Siul2_Dio_Ip_WritePin(LED_PORT, LED_PIN, 1U); /* 运行到此处说明发生错误 */
}
}
/* app_linker */
MEMORY
{
int_flash : ORIGIN = 0x00400000 + 0x00010000 + 0x200, LENGTH = 0x001D4000 - 0x00010000 - 0x200 /* 2048K - 176K (sBAF + HSE)*/
int_itcm : ORIGIN = 0x00000000, LENGTH = 0x00008000 /* 32K */
int_dtcm : ORIGIN = 0x20000000, LENGTH = 0x00010000 /* 64K */
int_sram : ORIGIN = 0x20400000, LENGTH = 0x00006F00 /* 27 KB */
int_sram_fls_rsv : ORIGIN = 0x20406F00, LENGTH = 0x00000100
int_sram_stack_c0 : ORIGIN = 0x20407000, LENGTH = 0x00001000
int_sram_no_cacheable : ORIGIN = 0x20408000, LENGTH = 0x00007F00 /* 32kb , needs to include int_results */
int_sram_results : ORIGIN = 0x2040FF00, LENGTH = 0x00000100
int_sram_shareable : ORIGIN = 0x20410000, LENGTH = 0x00008000 /* 32KB */
ram_rsvd2 : ORIGIN = 0x20418000, LENGTH = 0 /* End of SRAM */
}
/* app_main.c */
void TestDelay(uint32 delay);
void TestDelay(uint32 delay)
{
static volatile uint32 DelayTimer = 0;
while (DelayTimer<delay)
{
DelayTimer++;
}
DelayTimer=0;
}
/**
* @brief Main function of the example
* @details Initializez the used drivers and uses the Icu
* and Dio drivers to toggle a LED on a push button
*/
int main(void)
{
/* Initialize all pins using the Port driver */
Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);
while (1)
{
Siul2_Dio_Ip_WritePin(LED_PORT, LED_PIN, 1U);
TestDelay(4800000);
Siul2_Dio_Ip_WritePin(LED_PORT, LED_PIN, 0U);
TestDelay(4800000);
}
//Exit_Example(TRUE);
return (0U);
}