Get specified temperature range for S32K116

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Get specified temperature range for S32K116

ソリューションへジャンプ
1,019件の閲覧回数
markus1
Contributor II

I'm using a S32K116 MCU with extended temperature range (-40...125°C) for my current project. I would like to detect if a wrong chip with the lower temperature range is assembled, because this could lead to expensive loss of function in the field.

Is there a register inside the chip that contains the temperature range information like the registers that contain information about the chip features (SIM->SDID)?

If not, is there some other way to detect the specified temperature range in software?

Thanks,

Markus

ラベル(1)
0 件の賞賛
1 解決策
931件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I don't think it would be possible to detect it SW way. Such information is not stored in any MCU's register.

元の投稿で解決策を見る

0 件の賞賛
1 返信
932件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I don't think it would be possible to detect it SW way. Such information is not stored in any MCU's register.

0 件の賞賛