Flash read and Write, Memory mapping of S32K118

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash read and Write, Memory mapping of S32K118

2,577件の閲覧回数
ambarishhundeka
Contributor III

Hello All,

kindly provide me the sample code for flash read and write operation(need it for bootloader development).

1. Flash read and write of S32K118

2. memory mapping or layout (flash memory segmentation) OF S32K118 .

3. IVT Area(address details)

4. Interval timer sample code (timer configuration)

Thanks in advance.

Regards,

AMBARISH

ラベル(1)
0 件の賞賛
返信
1 返信

1,665件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

We don’t have any Flash example code ported on S32K118,

However, you can refer to Example S32K144 Flash RW simple.

 

The memory map and the interrupt vector table are both attached to the Reference manual (S32K1xx_memory_map.xlsx, S32K1xx_DMA_Interrupt_mapping.xlsx).

 

Regards,

Daniel

0 件の賞賛
返信