Flash read and Write, Memory mapping of S32K118

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash read and Write, Memory mapping of S32K118

2,490 Views
ambarishhundeka
Contributor III

Hello All,

kindly provide me the sample code for flash read and write operation(need it for bootloader development).

1. Flash read and write of S32K118

2. memory mapping or layout (flash memory segmentation) OF S32K118 .

3. IVT Area(address details)

4. Interval timer sample code (timer configuration)

Thanks in advance.

Regards,

AMBARISH

Labels (1)
0 Kudos
Reply
1 Reply

1,578 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

We don’t have any Flash example code ported on S32K118,

However, you can refer to Example S32K144 Flash RW simple.

 

The memory map and the interrupt vector table are both attached to the Reference manual (S32K1xx_memory_map.xlsx, S32K1xx_DMA_Interrupt_mapping.xlsx).

 

Regards,

Daniel

0 Kudos
Reply