Hi, I need inputs on the following:
1. Which port needs to be connected from U-Multilink debugger to S32K118EVB-Q064, for flashing and debugging?
2. If I need to use an adapter to power up the board, what should be the ampere rating?
3. What tool or driver should I install in order to work with the board and debugger? I did not get any driver installation prompt when I connected the debugger. Also, once I connect the board to the PC, what's the next step?
Any information is appreciated.
Thank you in advance!
1.If you have to use U-Multilink, please check J14 SWD connecter.(also OpenSDA USB can be used for debugging and flashing)
2.12V & less than 5A adapter will be fine.
3.Have you readed Get Started with the S32K118EVB
You can click this link for this file.
and I suggest you install S32 Design Studio for Arm 2.2 & Updates RTM 3.0.3
BR!
Jim,
Hi Jim,
Thank you for the input.
But when I try with the OpenSDA USB, I am getting error. The screenshot of the configuration and the error are attached.
I installed the GDA server plugins. As given in the link https://www.nxp.com/document/guide/get-started-with-the-s32k118evb:GS-S32K118EVB the board should be up and the RGB shall blink, right? But that is not working too. The J107 is in 3-2 position. Is there anything else that needs to be done to run the application on the board?
Also, I need the procedure to download a sample code from the S32DS on to the board using the OpenSDA USB. Because I tried the ways I understood, including as mentioned above, and there's no luck yet.
This is my first time with the board, so please excuse if I have been following some wrong procedure or approach.
Looking forward for inputs.
Thank you!