Connection of S32K118EVB-Q064 with U-Multilink Rev.D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connection of S32K118EVB-Q064 with U-Multilink Rev.D

653 Views
rahulpkumar-2612
Contributor II

Hi, I need inputs on the following:

1. Which port needs to be connected from U-Multilink debugger to S32K118EVB-Q064, for flashing and debugging?

2. If I need to use an adapter to power up the board, what should be the ampere rating?

3. What tool or driver should I install in order to work with the board and debugger? I did not get any driver installation prompt when I connected the debugger. Also, once I connect the board to the PC, what's the next step?

Any information is appreciated.

 

Thank  you in advance!

 

0 Kudos
3 Replies

642 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@rahulpkumar-2612

1.If you have to use U-Multilink, please check J14 SWD connecter.(also OpenSDA USB can be used for debugging and flashing)

 

                                       Senlent_0-1641264032458.png

2.12V & less than 5A adapter will be fine.

 

3.Have you readed Get Started with the S32K118EVB

You can click this link for this file.

https://www.nxp.com/design/development-boards/automotive-development-platforms/s32k-mcu-platforms/s3...

 

and I suggest you install S32 Design Studio for Arm 2.2 & Updates RTM 3.0.3

https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for...

 

BR!

     Jim,

 

0 Kudos

631 Views
rahulpkumar-2612
Contributor II

Hi Jim,

Thank you for the input.

But when I try with the OpenSDA USB, I am getting error. The screenshot of the configuration and the error are attached.

I installed the GDA server plugins. As given in the link https://www.nxp.com/document/guide/get-started-with-the-s32k118evb:GS-S32K118EVB the board should be up and the RGB shall blink, right? But that is not working too. The J107 is in 3-2 position. Is there anything else that needs to be done to run the application on the board?

Also, I need the procedure to download a sample code from the S32DS on to the board using the OpenSDA USB. Because I tried the ways I understood, including as mentioned above, and there's no luck yet.

This is my first time with the board, so please excuse if I have been following some wrong procedure or approach.

Looking forward for inputs.

Thank you!

0 Kudos

620 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@rahulpkumar-2612

Please try to use GDB PEMicro Interface Debugging.

Senlent_0-1641282881290.png

and be sure choice the right  Power Jumper.

Senlent_1-1641283027444.png

BR!

      Jim,

0 Kudos