Dear NXP Support Team,
I am currently working on a Battery Management System (BMS) using the S32K144 microcontroller and would like to better understand the differences between the MC33772B and MC33772C when integrated into such a system. Specifically, I have the following questions:
What are the main differences between the MC33772B and MC33772C in terms of measurement and monitoring capabilities when connected to the S32K144 via SPI communication?
Are there any changes in the communication protocol or performance?
In terms of battery protection features (over-temperature, over-current, over-voltage, etc.), what improvements does the MC33772C offer compared to the MC33772B?
How do these changes impact the integration and operation with the S32K144?
Is the MC33772C backward compatible with existing configurations using the MC33772B on the S32K144?
Does upgrading from MC33772B to MC33772C require significant software or hardware changes?
How do the differences in accuracy for voltage, current, and temperature measurements between the MC33772B and MC33772C impact battery control and protection in the BMS?
I appreciate your assistance and look forward to your response to help guide my component selection for the project.
Best regards,
Son Thai