Changes to the p_flash of the S32K312 may cause the program to run erratically.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changes to the p_flash of the S32K312 may cause the program to run erratically.

113件の閲覧回数
victory
Contributor III

Hi,nxp

1.By modifying the linker_flash_s32k312.ld file, the starting address of p_flash was changed from 0x00400000 to 0x00440200, resulting in the program malfunctioning, as shown in the attached image. The code is included in the attachment.

victory_1-1724139888319.png

2.The expected outcome is that the program does not feed the watchdog and should restart from the beginning, rather than malfunctioning.

That's all, thank you.

 

0 件の賞賛
返信
5 返答(返信)

74件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @victory,

I understand that this project should be flashed by a bootloader, right?

But if you flash the project directly (DM181S_S32K312_BOOT.elf), the SBAF then searches for the first valid IVT starting from the lowest address at 0x00400000.

danielmartynek_0-1724221857960.png

 

Regards,

Daniel

 

0 件の賞賛
返信

68件の閲覧回数
victory
Contributor III

Hi,danielmartnek

1.I understand that this project should be flashed by a bootloader, right?

Reply:Yes,There are other matters to pay attention to.

2.But if you flash the project directly (DM181S_S32K312_BOOT.elf), the SBAF then searches for the first valid IVT starting from the lowest address at 0x00400000.

ReplyAccording to your intention, when debugging the app project online without the bootloader, the starting address of int_pflash still needs to be set to 0x00400000.

3.Additionally, if we enable the HSE firmware later on, how should we debug the app project that does not include the bootloader, and how do we allocate memory?

0 件の賞賛
返信

59件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

You can place it at 0x50_0000, which is a valid IVT address and it is in the next block, so it can be programmed by the bootloader in the 0x40_0000 block.

danielmartynek_0-1724237036105.png

 

Regarding the HSE_FW, please create a new thread.

 

Thank you,

BR, Daniel

0 件の賞賛
返信

55件の閲覧回数
victory
Contributor III

I modified the original project by changing the starting address of int_pflash to 0x00500000 in the linker_flash_s32k312.ld file, but the program still runs incorrectly. Am I misunderstanding something, or is there another area that I haven't changed?

1)linker_flash_s32k312.ld->MEMORY

victory_2-1724239588791.png

2)Schematic of program malfunction

victory_0-1724239499481.png

 

0 件の賞賛
返信

14件の閲覧回数
victory
Contributor III

Hi,

Erase the entire chip and reload the program.

Thanks

0 件の賞賛
返信